<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Adc_example_S32K344 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Adc-example-S32K344/m-p/1697640#M25712</link>
    <description>&lt;P&gt;Which package I should install to have &lt;STRONG&gt;Adc_example_S32K344&lt;/STRONG&gt; available.&lt;/P&gt;&lt;P&gt;I have&amp;nbsp;S32K3X4EVB-Q172 board and have installed:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;SW32K3xx.S32DS_3.5.0_D2303.zip,&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;SW32K3_RTD_4.4_R21-11_3.0.0_CD04_D2212_updatesite.zip, and&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;SW32K3_RTD_R21-11_3.0.0_P07_D2306_DS_updatesite.zip,&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I only see&amp;nbsp;Adc_example_S32K311 available.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Gary&lt;/P&gt;&lt;P&gt;I am able to get Adc_example_S32K344 now after install "SW32K3_RTD4.4_R21-11_3.0.0_D2303",&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Issue:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;When I build: "&lt;STRONG&gt;Adc_example_S32K344&lt;/STRONG&gt;"&amp;nbsp;or "&lt;STRONG&gt;Clock_Lp_Example_S32K344&lt;/STRONG&gt;"&lt;/P&gt;&lt;P&gt;I have the same Error of "&lt;STRONG&gt;Pins initialization requires the PINS Driver in the project&lt;/STRONG&gt;" after I enable the Pins configuration,&lt;/P&gt;&lt;P&gt;But I can build "&lt;STRONG&gt;Port_Example_S32K344&lt;/STRONG&gt;" without error.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any advice?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Gary&lt;/P&gt;</description>
    <pubDate>Fri, 04 Aug 2023 19:10:53 GMT</pubDate>
    <dc:creator>GaryZhang1</dc:creator>
    <dc:date>2023-08-04T19:10:53Z</dc:date>
    <item>
      <title>Adc_example_S32K344</title>
      <link>https://community.nxp.com/t5/S32K/Adc-example-S32K344/m-p/1697640#M25712</link>
      <description>&lt;P&gt;Which package I should install to have &lt;STRONG&gt;Adc_example_S32K344&lt;/STRONG&gt; available.&lt;/P&gt;&lt;P&gt;I have&amp;nbsp;S32K3X4EVB-Q172 board and have installed:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;SW32K3xx.S32DS_3.5.0_D2303.zip,&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;SW32K3_RTD_4.4_R21-11_3.0.0_CD04_D2212_updatesite.zip, and&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;SW32K3_RTD_R21-11_3.0.0_P07_D2306_DS_updatesite.zip,&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I only see&amp;nbsp;Adc_example_S32K311 available.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Gary&lt;/P&gt;&lt;P&gt;I am able to get Adc_example_S32K344 now after install "SW32K3_RTD4.4_R21-11_3.0.0_D2303",&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Issue:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;When I build: "&lt;STRONG&gt;Adc_example_S32K344&lt;/STRONG&gt;"&amp;nbsp;or "&lt;STRONG&gt;Clock_Lp_Example_S32K344&lt;/STRONG&gt;"&lt;/P&gt;&lt;P&gt;I have the same Error of "&lt;STRONG&gt;Pins initialization requires the PINS Driver in the project&lt;/STRONG&gt;" after I enable the Pins configuration,&lt;/P&gt;&lt;P&gt;But I can build "&lt;STRONG&gt;Port_Example_S32K344&lt;/STRONG&gt;" without error.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any advice?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Gary&lt;/P&gt;</description>
      <pubDate>Fri, 04 Aug 2023 19:10:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Adc-example-S32K344/m-p/1697640#M25712</guid>
      <dc:creator>GaryZhang1</dc:creator>
      <dc:date>2023-08-04T19:10:53Z</dc:date>
    </item>
    <item>
      <title>Re: Adc_example_S32K344</title>
      <link>https://community.nxp.com/t5/S32K/Adc-example-S32K344/m-p/1697669#M25713</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@GaryZhang1" target="_blank"&gt;Hi@GaryZhang1&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;from my side,&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Senlent_0-1690983120246.png" style="width: 506px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/234777iA26C2A5C6683B73B/image-dimensions/506x443?v=v2" width="506" height="443" role="button" title="Senlent_0-1690983120246.png" alt="Senlent_0-1690983120246.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Senlent_0-1690983120246.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 02 Aug 2023 13:33:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Adc-example-S32K344/m-p/1697669#M25713</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2023-08-02T13:33:01Z</dc:date>
    </item>
    <item>
      <title>Re: Adc_example_S32K344</title>
      <link>https://community.nxp.com/t5/S32K/Adc-example-S32K344/m-p/1697775#M25718</link>
      <description>Thanks for the reply.</description>
      <pubDate>Wed, 02 Aug 2023 16:12:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Adc-example-S32K344/m-p/1697775#M25718</guid>
      <dc:creator>GaryZhang1</dc:creator>
      <dc:date>2023-08-02T16:12:39Z</dc:date>
    </item>
    <item>
      <title>Re: Adc_example_S32K344</title>
      <link>https://community.nxp.com/t5/S32K/Adc-example-S32K344/m-p/1702330#M25912</link>
      <description>&lt;P&gt;This is no longer an issue after updated the main.c code., thanks -- Gary&lt;/P&gt;</description>
      <pubDate>Wed, 09 Aug 2023 19:40:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Adc-example-S32K344/m-p/1702330#M25912</guid>
      <dc:creator>GaryZhang1</dc:creator>
      <dc:date>2023-08-09T19:40:47Z</dc:date>
    </item>
  </channel>
</rss>