<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 RAppID_BL via Vector CANCaseXL</title>
    <link>https://community.nxp.com/t5/S32K/RAppID-BL-via-Vector-CANCaseXL/m-p/1697165#M25683</link>
    <description>&lt;P&gt;Dear Sir,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am trying to flash the simple FlexCAN0 project *.SREC file over CAN bus via GUI of RAppID_BL.&lt;/P&gt;&lt;P&gt;The hardware board is customized with S32K144 LQFP-64, normal functional tested via PEmicro flashed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;SREC build Pre-Test :&lt;/P&gt;&lt;P&gt;1) Complied the FlexCAN0 project modified from example to send out CAN in PTC2 &amp;amp; PTC3 instead.&amp;nbsp;&lt;/P&gt;&lt;P&gt;2) Flashed via PEmicro tested it work fine.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;RBL configuration :&lt;/P&gt;&lt;P&gt;[FORMAT_VERSION]&lt;BR /&gt;3&lt;/P&gt;&lt;P&gt;[COMMUNICATION_SETUP]&lt;BR /&gt;Vector CANcaseXL, CH 1, 500K&lt;/P&gt;&lt;P&gt;[MCU_SETUP]&lt;BR /&gt;S32K144&lt;/P&gt;&lt;P&gt;[BAM_SETUP]&lt;BR /&gt;Disabled&lt;/P&gt;&lt;P&gt;[FILE_INFO]&lt;BR /&gt;C:\SVN_Checkout\S32DS_ARM2.2\S32K144_Project_FlexCan\Debug\S32K144_Project_FlexCan.srec, 0x0, 0x950, Checked&lt;/P&gt;&lt;P&gt;[OP_SETUP]&lt;BR /&gt;EraseProgram&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CAN Flash Testing :&lt;/P&gt;&lt;P&gt;1) Load RBL file -&amp;nbsp;C:\Freescale\RAppIDBL\RAppidBL_Vector_CANCaseXL.rbl&lt;/P&gt;&lt;P&gt;2) Error - Loss Communication&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If any idea what setup I am doing wrongly ?&lt;/P&gt;&lt;P&gt;Or do you guy have any simple project working for testing&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Narudol T.&lt;/P&gt;</description>
    <pubDate>Wed, 02 Aug 2023 04:22:36 GMT</pubDate>
    <dc:creator>narudoltatiyava</dc:creator>
    <dc:date>2023-08-02T04:22:36Z</dc:date>
    <item>
      <title>RAppID_BL via Vector CANCaseXL</title>
      <link>https://community.nxp.com/t5/S32K/RAppID-BL-via-Vector-CANCaseXL/m-p/1697165#M25683</link>
      <description>&lt;P&gt;Dear Sir,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am trying to flash the simple FlexCAN0 project *.SREC file over CAN bus via GUI of RAppID_BL.&lt;/P&gt;&lt;P&gt;The hardware board is customized with S32K144 LQFP-64, normal functional tested via PEmicro flashed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;SREC build Pre-Test :&lt;/P&gt;&lt;P&gt;1) Complied the FlexCAN0 project modified from example to send out CAN in PTC2 &amp;amp; PTC3 instead.&amp;nbsp;&lt;/P&gt;&lt;P&gt;2) Flashed via PEmicro tested it work fine.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;RBL configuration :&lt;/P&gt;&lt;P&gt;[FORMAT_VERSION]&lt;BR /&gt;3&lt;/P&gt;&lt;P&gt;[COMMUNICATION_SETUP]&lt;BR /&gt;Vector CANcaseXL, CH 1, 500K&lt;/P&gt;&lt;P&gt;[MCU_SETUP]&lt;BR /&gt;S32K144&lt;/P&gt;&lt;P&gt;[BAM_SETUP]&lt;BR /&gt;Disabled&lt;/P&gt;&lt;P&gt;[FILE_INFO]&lt;BR /&gt;C:\SVN_Checkout\S32DS_ARM2.2\S32K144_Project_FlexCan\Debug\S32K144_Project_FlexCan.srec, 0x0, 0x950, Checked&lt;/P&gt;&lt;P&gt;[OP_SETUP]&lt;BR /&gt;EraseProgram&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CAN Flash Testing :&lt;/P&gt;&lt;P&gt;1) Load RBL file -&amp;nbsp;C:\Freescale\RAppIDBL\RAppidBL_Vector_CANCaseXL.rbl&lt;/P&gt;&lt;P&gt;2) Error - Loss Communication&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If any idea what setup I am doing wrongly ?&lt;/P&gt;&lt;P&gt;Or do you guy have any simple project working for testing&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Narudol T.&lt;/P&gt;</description>
      <pubDate>Wed, 02 Aug 2023 04:22:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/RAppID-BL-via-Vector-CANCaseXL/m-p/1697165#M25683</guid>
      <dc:creator>narudoltatiyava</dc:creator>
      <dc:date>2023-08-02T04:22:36Z</dc:date>
    </item>
  </channel>
</rss>