<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K3 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K3/m-p/1696975#M25671</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have installed DS version 3.4 and S32K3XX DEVELOPMENT PACKAGE and&amp;nbsp;S32K3 Real-Time Drivers AUTOSAR 4.4 Version 2.0.0 and&amp;nbsp;&amp;nbsp;GCC 9.2 and GNUARM PEMICRO INTERFACE DEBUGGING SUPPORT.&lt;/P&gt;&lt;P&gt;I can build the examples by S32DS PROJEDTS FROM EXAMPLE tab.&lt;/P&gt;&lt;P&gt;However I couldn't flash the code nor debug the project.. for instance take a project called&lt;/P&gt;&lt;P&gt;"Dio_Example_S32k3xx" I use a debug configuration called "Dio_Example_S32k3xx "Dio_Example_S32k3xx_debug_flash_ PNE".&lt;/P&gt;&lt;P&gt;WITH THIS DEBUG CONFIGURATION , open sda does not even connect to the target&amp;nbsp; and When I use JTAG and PNE debugger it connects to the target and then display a "run time error" message and debugging terminates. I'm using&amp;nbsp; a S32K1XEVAL-Q100 Board.&lt;/P&gt;&lt;P&gt;Please help me to resolve this.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Koorosh Hajiani&lt;/P&gt;</description>
    <pubDate>Tue, 01 Aug 2023 20:44:19 GMT</pubDate>
    <dc:creator>hajianik</dc:creator>
    <dc:date>2023-08-01T20:44:19Z</dc:date>
    <item>
      <title>S32K3</title>
      <link>https://community.nxp.com/t5/S32K/S32K3/m-p/1696975#M25671</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have installed DS version 3.4 and S32K3XX DEVELOPMENT PACKAGE and&amp;nbsp;S32K3 Real-Time Drivers AUTOSAR 4.4 Version 2.0.0 and&amp;nbsp;&amp;nbsp;GCC 9.2 and GNUARM PEMICRO INTERFACE DEBUGGING SUPPORT.&lt;/P&gt;&lt;P&gt;I can build the examples by S32DS PROJEDTS FROM EXAMPLE tab.&lt;/P&gt;&lt;P&gt;However I couldn't flash the code nor debug the project.. for instance take a project called&lt;/P&gt;&lt;P&gt;"Dio_Example_S32k3xx" I use a debug configuration called "Dio_Example_S32k3xx "Dio_Example_S32k3xx_debug_flash_ PNE".&lt;/P&gt;&lt;P&gt;WITH THIS DEBUG CONFIGURATION , open sda does not even connect to the target&amp;nbsp; and When I use JTAG and PNE debugger it connects to the target and then display a "run time error" message and debugging terminates. I'm using&amp;nbsp; a S32K1XEVAL-Q100 Board.&lt;/P&gt;&lt;P&gt;Please help me to resolve this.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Koorosh Hajiani&lt;/P&gt;</description>
      <pubDate>Tue, 01 Aug 2023 20:44:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3/m-p/1696975#M25671</guid>
      <dc:creator>hajianik</dc:creator>
      <dc:date>2023-08-01T20:44:19Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3</title>
      <link>https://community.nxp.com/t5/S32K/S32K3/m-p/1699370#M25780</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/138997"&gt;@hajianik&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;According to your description, you use S32K3 RTD and S32K1 board.&lt;/P&gt;
&lt;P&gt;If this is a typo, and it is an S32K3 board, then, there is no OpenSDA debugger.&lt;/P&gt;
&lt;P&gt;Can you clarify?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 04 Aug 2023 11:28:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3/m-p/1699370#M25780</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2023-08-04T11:28:54Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3</title>
      <link>https://community.nxp.com/t5/S32K/S32K3/m-p/1699494#M25786</link>
      <description>&lt;P&gt;Hi Daniel,&lt;/P&gt;&lt;P&gt;It is a typo and I use&amp;nbsp;&lt;SPAN&gt;S32K3-q100 board. on this board the processor is s32k311q100 however the examples are&amp;nbsp;&amp;nbsp; targeted for a s32k312_q172 micro .when I use these examples that are&amp;nbsp; for&amp;nbsp;s32k312_q172 I get a&amp;nbsp; an exception in start_up code, that is when I use external power supply and PNE debugger.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;There is no support in DESIGN STUDIO V3.4 for s32k311 or 310 series&amp;nbsp; &amp;nbsp;. WHAT CAN I DO?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 04 Aug 2023 15:31:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3/m-p/1699494#M25786</guid>
      <dc:creator>hajianik</dc:creator>
      <dc:date>2023-08-04T15:31:01Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3</title>
      <link>https://community.nxp.com/t5/S32K/S32K3/m-p/1700049#M25805</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/138997"&gt;@hajianik&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;There is support for S32K311 in S32DS IDE v3.5, RTD 3.0.0&lt;/P&gt;
&lt;P&gt;There are no RTD examples for S32K311, but a new RTD project for S32K311 can be created.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1691397951334.png" style="width: 742px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/235302i6AA11AF76D8050B6/image-dimensions/742x147?v=v2" width="742" height="147" role="button" title="danielmartynek_0-1691397951334.png" alt="danielmartynek_0-1691397951334.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;danielmartynek_0-1691397951334.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 07 Aug 2023 08:46:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3/m-p/1700049#M25805</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2023-08-07T08:46:51Z</dc:date>
    </item>
  </channel>
</rss>