<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32K144EVB Secure Boot</title>
    <link>https://community.nxp.com/t5/S32K/S32K144EVB-Secure-Boot/m-p/787092#M2556</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried and&amp;nbsp;the BOOT_SIZE is counted in number of bits, rounded up to the nearest 128-bits.&amp;nbsp; i.e. Option (1) in my original post.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 20 Aug 2018 13:33:22 GMT</pubDate>
    <dc:creator>bix010</dc:creator>
    <dc:date>2018-08-20T13:33:22Z</dc:date>
    <item>
      <title>S32K144EVB Secure Boot</title>
      <link>https://community.nxp.com/t5/S32K/S32K144EVB-Secure-Boot/m-p/787090#M2554</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying out the secure boot feature on the S32K144EVB board. I'm being careful, as&amp;nbsp;I don't want to&amp;nbsp;brick the board. I'm seeing two different options for boot size:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. In the sample code provided in AN5401SW, example #4 shows how to configure secure boot manually.&amp;nbsp; It sets the BOOT_SIZE to 128*1024*8.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. In the SDK code for CSEC module provided by Processor Expert, the comments indicate the bootSize is the number of blocks of 128-bit data to check on boot. Maximum size is 512KB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Based on (2), would the maximum bootSize be equals to (512KB / 128bit) = 4096?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But in (1), the BOOT_SIZE is defined as 128*1024*8 = 1,048,576.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the correct way to calculate the boot size?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Jul 2018 06:33:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144EVB-Secure-Boot/m-p/787090#M2554</guid>
      <dc:creator>bix010</dc:creator>
      <dc:date>2018-07-26T06:33:46Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144EVB Secure Boot</title>
      <link>https://community.nxp.com/t5/S32K/S32K144EVB-Secure-Boot/m-p/787091#M2555</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;the 512K is a read parittion, cmac can't caculate over a partition.&lt;/P&gt;&lt;P&gt;caculate:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;16byte=128bits/8bits&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;512*1024byte/16byte=32768 blocks.(max)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Aug 2018 06:50:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144EVB-Secure-Boot/m-p/787091#M2555</guid>
      <dc:creator>fuzeng</dc:creator>
      <dc:date>2018-08-16T06:50:09Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144EVB Secure Boot</title>
      <link>https://community.nxp.com/t5/S32K/S32K144EVB-Secure-Boot/m-p/787092#M2556</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried and&amp;nbsp;the BOOT_SIZE is counted in number of bits, rounded up to the nearest 128-bits.&amp;nbsp; i.e. Option (1) in my original post.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Aug 2018 13:33:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144EVB-Secure-Boot/m-p/787092#M2556</guid>
      <dc:creator>bix010</dc:creator>
      <dc:date>2018-08-20T13:33:22Z</dc:date>
    </item>
  </channel>
</rss>