<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Siul2_Dio_Ip_Example_S32K312 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Siul2-Dio-Ip-Example-S32K312/m-p/1693743#M25487</link>
    <description>Now the s32k314 project is created, but the debug flash is faulty.&lt;BR /&gt;Emulation stops at the cpsid i location in the file startup_cm7.s</description>
    <pubDate>Thu, 27 Jul 2023 03:28:46 GMT</pubDate>
    <dc:creator>Lita</dc:creator>
    <dc:date>2023-07-27T03:28:46Z</dc:date>
    <item>
      <title>Siul2_Dio_Ip_Example_S32K312</title>
      <link>https://community.nxp.com/t5/S32K/Siul2-Dio-Ip-Example-S32K312/m-p/1691228#M25337</link>
      <description>&lt;P&gt;&lt;SPAN&gt;After Siul2_Dio_Ip_Example_S32K312 routine is burned to S32K314, it is burned to flash through jlink, and an error occurs. K314 is designed by referring to the development board of the official website.&lt;/SPAN&gt;The following error occurs：&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;ownloading 16224 bytes @ address 0x00400000 - Verified OK&lt;BR /&gt;Downloading 6648 bytes @ address 0x00403F60 - Verified OK&lt;BR /&gt;Downloading 148 bytes @ address 0x00405958 - Verified OK&lt;BR /&gt;Downloading 1036 bytes @ address 0x004059EC - Verified OK&lt;BR /&gt;Comparing flash [....................] Done.&lt;BR /&gt;Erasing flash [....................] Done.&lt;BR /&gt;Programming flash [....................] Done.&lt;BR /&gt;Writing register (PC = 0x 401420)&lt;BR /&gt;Read 4 bytes @ address 0x00401420 (Data = 0xF04FB672)&lt;BR /&gt;Read 2 bytes @ address 0x00401420 (Data = 0xB672)&lt;BR /&gt;Reading 64 bytes @ address 0x004015C0&lt;BR /&gt;Read 2 bytes @ address 0x004015E8 (Data = 0xB538)&lt;BR /&gt;Received monitor command: clrbp&lt;BR /&gt;Received monitor command: reset&lt;BR /&gt;Resetting target&lt;BR /&gt;Received monitor command: halt&lt;BR /&gt;Halting target CPU...&lt;BR /&gt;...Target halted (PC = 0x20000340)&lt;BR /&gt;Read 2 bytes @ address 0x004015E8 (Data = 0xB538)&lt;BR /&gt;Received monitor command: regs&lt;BR /&gt;R0 = 200005EC, R1 = 20000634, R2 = 2000060C, R3 = 00405C00&lt;BR /&gt;R4 = 200005EC, R5 = 20000644, R6 = 20000644, R7 = 00000000&lt;BR /&gt;R8 = 00000000, R9 = 00000000, R10= 00000000, R11= 00000000&lt;BR /&gt;R12= 20000570, R13= 200005E0, MSP= 200005E0, PSP= 00000000&lt;BR /&gt;R14(LR) = 20000341, R15(PC) = 20000340&lt;BR /&gt;XPSR 21000003, APSR 20000000, EPSR 01000000, IPSR 00000003&lt;BR /&gt;CFBP 00000001, CONTROL 00, FAULTMASK 00, BASEPRI 00, PRIMASK 01&lt;/P&gt;&lt;P&gt;Security extension regs:&lt;BR /&gt;MSP_S = 00000000, MSPLIM_S = 00000000&lt;BR /&gt;PSP_S = 00000000, PSPLIM_S = 00000000&lt;BR /&gt;MSP_NS = 200005E0, MSPLIM_NS = 00000000&lt;BR /&gt;PSP_NS = 00000000, PSPLIM_NS = 00000000&lt;BR /&gt;CONTROL_S 00, FAULTMASK_S 00, BASEPRI_S 00, PRIMASK_S 00&lt;BR /&gt;CONTROL_NS 00, FAULTMASK_NS 00, BASEPRI_NS 00, PRIMASK_NS 01&lt;/P&gt;&lt;P&gt;Reading all registers&lt;BR /&gt;Setting breakpoint @ address 0x004015E8, Size = 2, BPHandle = 0x0001&lt;BR /&gt;Starting target CPU...&lt;BR /&gt;...Target halted (DBGRQ, PC = 0x20010000)&lt;BR /&gt;Reading all registers&lt;BR /&gt;Removing breakpoint @ address 0x004015E8, Size = 2&lt;BR /&gt;WARNING: Failed to read memory @ address 0x20010000&lt;BR /&gt;Reading 64 bytes @ address 0x00000000&lt;BR /&gt;Reading 64 bytes @ address 0x00000040&lt;BR /&gt;Reading 64 bytes @ address 0x00000080&lt;BR /&gt;Reading 64 bytes @ address 0x20010000&lt;BR /&gt;WARNING: Failed to read memory @ address 0x20010000&lt;BR /&gt;WARNING: Failed to read memory @ address 0x20010000&lt;BR /&gt;Reading 64 bytes @ address 0x2000FFC0&lt;BR /&gt;Read 4 bytes @ address 0x20000340 (Data = 0x00000000)&lt;BR /&gt;Read 2 bytes @ address 0x20000340 (Data = 0x0000)&lt;BR /&gt;Read 4 bytes @ address 0x20000340 (Data = 0x00000000)&lt;BR /&gt;Read 2 bytes @ address 0x20000340 (Data = 0x0000)&lt;BR /&gt;Reading 64 bytes @ address 0x20010000&lt;BR /&gt;WARNING: Failed to read memory @ address 0x20010000&lt;BR /&gt;WARNING: Failed to read memory @ address 0x20010000&lt;BR /&gt;Reading 64 bytes @ address 0x20010000&lt;BR /&gt;WARNING: Failed to read memory @ address 0x20010000&lt;BR /&gt;WARNING: Failed to read memory @ address 0x20010002&lt;BR /&gt;Reading 64 bytes @ address 0x20010000&lt;BR /&gt;WARNING: Failed to read memory @ address 0x20010000&lt;BR /&gt;WARNING: Failed to read memory @ address 0x20010000&lt;BR /&gt;Reading 64 bytes @ address 0x20010000&lt;BR /&gt;WARNING: Failed to read memory @ address 0x20010000&lt;BR /&gt;WARNING: Failed to read memory @ address 0x20010002&lt;BR /&gt;Reading 64 bytes @ address 0x2000FF80&lt;/P&gt;</description>
      <pubDate>Mon, 24 Jul 2023 09:00:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Siul2-Dio-Ip-Example-S32K312/m-p/1691228#M25337</guid>
      <dc:creator>Lita</dc:creator>
      <dc:date>2023-07-24T09:00:20Z</dc:date>
    </item>
    <item>
      <title>Re: Siul2_Dio_Ip_Example_S32K312</title>
      <link>https://community.nxp.com/t5/S32K/Siul2-Dio-Ip-Example-S32K312/m-p/1691232#M25338</link>
      <description>&lt;P&gt;The disassembly&amp;nbsp;print information as follows&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2000fffc: movs r0, r0&lt;BR /&gt;2000fffe: movs r0, r0&lt;BR /&gt;20010000: Failed to execute MI command:&lt;BR /&gt;-data-disassemble -s 536936448 -e 536936518 -- 3&lt;BR /&gt;Error message from debugger back end:&lt;BR /&gt;Cannot access memory at address 0x20010000&lt;BR /&gt;20010001: Failed to execute MI command:&lt;BR /&gt;-data-disassemble -s 536936449 -e 536936597 -- 3&lt;BR /&gt;Error message from debugger back end:&lt;BR /&gt;Cannot access memory at address 0x20010000&lt;BR /&gt;20010002: Failed to execute MI command:&lt;BR /&gt;-data-disassemble -s 536936450 -e 536936598 -- 3&lt;BR /&gt;Error message from debugger back end:&lt;/P&gt;</description>
      <pubDate>Mon, 24 Jul 2023 09:03:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Siul2-Dio-Ip-Example-S32K312/m-p/1691232#M25338</guid>
      <dc:creator>Lita</dc:creator>
      <dc:date>2023-07-24T09:03:02Z</dc:date>
    </item>
    <item>
      <title>Re: Siul2_Dio_Ip_Example_S32K312</title>
      <link>https://community.nxp.com/t5/S32K/Siul2-Dio-Ip-Example-S32K312/m-p/1692321#M25420</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/217547"&gt;@Lita&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The S32K312 is a different MCU.&lt;/P&gt;
&lt;P&gt;Please create a new project for S32K314 and refer to the S32K344 example.&lt;/P&gt;
&lt;P&gt;The S32K314 is a decoupled S32K344 with one core disabled.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jul 2023 13:44:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Siul2-Dio-Ip-Example-S32K312/m-p/1692321#M25420</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2023-07-25T13:44:53Z</dc:date>
    </item>
    <item>
      <title>Re: Siul2_Dio_Ip_Example_S32K312</title>
      <link>https://community.nxp.com/t5/S32K/Siul2-Dio-Ip-Example-S32K312/m-p/1693743#M25487</link>
      <description>Now the s32k314 project is created, but the debug flash is faulty.&lt;BR /&gt;Emulation stops at the cpsid i location in the file startup_cm7.s</description>
      <pubDate>Thu, 27 Jul 2023 03:28:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Siul2-Dio-Ip-Example-S32K312/m-p/1693743#M25487</guid>
      <dc:creator>Lita</dc:creator>
      <dc:date>2023-07-27T03:28:46Z</dc:date>
    </item>
    <item>
      <title>Re: Siul2_Dio_Ip_Example_S32K312</title>
      <link>https://community.nxp.com/t5/S32K/Siul2-Dio-Ip-Example-S32K312/m-p/1694003#M25503</link>
      <description>&lt;P&gt;Can you load, for example, this project?&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K314-DTCM1-Backdoor-RTD201-DS34-v2/ta-p/1689350" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K314-DTCM1-Backdoor-RTD201-DS34-v2/ta-p/1689350&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you,&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;</description>
      <pubDate>Thu, 27 Jul 2023 08:47:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Siul2-Dio-Ip-Example-S32K312/m-p/1694003#M25503</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2023-07-27T08:47:29Z</dc:date>
    </item>
    <item>
      <title>Re: Siul2_Dio_Ip_Example_S32K312</title>
      <link>https://community.nxp.com/t5/S32K/Siul2-Dio-Ip-Example-S32K312/m-p/1694083#M25512</link>
      <description>The DEBUG flash cannot run again with the following error message:&lt;BR /&gt;SEGGER J-Link GDB Server V7.88j Command Line Version&lt;BR /&gt;&lt;BR /&gt;JLinkARM.dll V7.88j (DLL compiled Jun 28 2023 13:39:15)&lt;BR /&gt;&lt;BR /&gt;Command line: -if jtag -device S32K314 -endian little -speed 1000 -port 2331 -swoport 2332 -telnetport 2333 -vd -ir -localhostonly 1 -singlerun -strict -timeout 0 -nogui&lt;BR /&gt;-----GDB Server start settings-----&lt;BR /&gt;GDBInit file: none&lt;BR /&gt;GDB Server Listening port: 2331&lt;BR /&gt;SWO raw output listening port: 2332&lt;BR /&gt;Terminal I/O port: 2333&lt;BR /&gt;Accept remote connection: localhost only&lt;BR /&gt;Generate logfile: off&lt;BR /&gt;Verify download: on&lt;BR /&gt;Init regs on start: on&lt;BR /&gt;Silent mode: off&lt;BR /&gt;Single run mode: on&lt;BR /&gt;Target connection timeout: 0 ms&lt;BR /&gt;------J-Link related settings------&lt;BR /&gt;J-Link Host interface: USB&lt;BR /&gt;J-Link script: none&lt;BR /&gt;J-Link settings file: none&lt;BR /&gt;------Target related settings------&lt;BR /&gt;Target device: S32K314&lt;BR /&gt;Target device parameters: none&lt;BR /&gt;Target interface: JTAG&lt;BR /&gt;Target interface speed: 1000kHz&lt;BR /&gt;Target endian: little&lt;BR /&gt;&lt;BR /&gt;Connecting to J-Link...&lt;BR /&gt;J-Link is connected.&lt;BR /&gt;Firmware: J-Link V9 compiled Dec 13 2022 11:14:50&lt;BR /&gt;Hardware: V9.60&lt;BR /&gt;S/N: 69664823&lt;BR /&gt;Feature(s): RDI, GDB, FlashDL, FlashBP, JFlash&lt;BR /&gt;Checking target voltage...&lt;BR /&gt;Target voltage: 3.31 V&lt;BR /&gt;Listening on TCP/IP port 2331&lt;BR /&gt;Connecting to target...&lt;BR /&gt;&lt;BR /&gt;J-Link found 1 JTAG device, Total IRLen = 8&lt;BR /&gt;JTAG ID: 0x0996001D (Cortex-M7)&lt;BR /&gt;Initializing CPU registers...Connected to target&lt;BR /&gt;Waiting for GDB connection...Connected to 0000:0000:0000:0000:0000:0000:0000:0001&lt;BR /&gt;GDB client (conn. 876) requested target.xml from GDB Server&lt;BR /&gt;Reading common registers: Read register 'r0' (4 bytes) from hardware: 0x00000000&lt;BR /&gt;Read register 'r1' (4 bytes) from hardware: 0x00000000&lt;BR /&gt;Read register 'r2' (4 bytes) from hardware: 0x00000000&lt;BR /&gt;Read register 'r3' (4 bytes) from hardware: 0x00000000&lt;BR /&gt;Read register 'r4' (4 bytes) from hardware: 0x00000000&lt;BR /&gt;Read register 'r5' (4 bytes) from hardware: 0x00000000&lt;BR /&gt;Read register 'r6' (4 bytes) from hardware: 0x00000000&lt;BR /&gt;Read register 'r7' (4 bytes) from hardware: 0x00000000&lt;BR /&gt;Read register 'r8' (4 bytes) from hardware: 0x00000000&lt;BR /&gt;Read register 'r9' (4 bytes) from hardware: 0x00000000&lt;BR /&gt;Read register 'r10' (4 bytes) from hardware: 0x00000000&lt;BR /&gt;Read register 'r11' (4 bytes) from hardware: 0x00000000&lt;BR /&gt;Read register 'r12' (4 bytes) from hardware: 0x00000000&lt;BR /&gt;Read register 'sp' (4 bytes) from hardware: 0x00000000&lt;BR /&gt;Read register 'lr' (4 bytes) from hardware: 0x00000000&lt;BR /&gt;Read register 'pc' (4 bytes) from hardware: 0x00000000&lt;BR /&gt;Read register 'xpsr' (4 bytes) from hardware: 0x00000001&lt;BR /&gt;Read 4 bytes @ address 0x00000000 (Data = 0x00000000)&lt;BR /&gt;Read 2 bytes @ address 0x00000000 (Data = 0x0000)&lt;BR /&gt;Received monitor command: speed 100&lt;BR /&gt;Target interface speed set to 100 kHz&lt;BR /&gt;Received monitor command: clrbp&lt;BR /&gt;Received monitor command: reset&lt;BR /&gt;Resetting target&lt;BR /&gt;Received monitor command: halt&lt;BR /&gt;Halting target CPU...&lt;BR /&gt;...Target halted (PC = 0x20000008)&lt;BR /&gt;Received monitor command: regs&lt;BR /&gt;R0 = 20404000, R1 = 00000000, R2 = DEADBEEF, R3 = 00400400&lt;BR /&gt;R4 = 200008B4, R5 = 200008D4, R6 = 200008D4, R7 = 00000000&lt;BR /&gt;R8 = 00000000, R9 = 00000000, R10= 00000000, R11= 00000000&lt;BR /&gt;R12= 00000FFE, R13= 200008A8, MSP= 200008A8, PSP= 00000000&lt;BR /&gt;R14(LR) = 2000035B, R15(PC) = 20000008&lt;BR /&gt;XPSR 61000000, APSR 60000000, EPSR 01000000, IPSR 00000000&lt;BR /&gt;CFBP 00000000, CONTROL 00, FAULTMASK 00, BASEPRI 00, PRIMASK 00&lt;BR /&gt;&lt;BR /&gt;Security extension regs:&lt;BR /&gt;MSP_S = 00000000, MSPLIM_S = 00000000&lt;BR /&gt;PSP_S = 00000000, PSPLIM_S = 00000000&lt;BR /&gt;MSP_NS = 200008A8, MSPLIM_NS = 00000000&lt;BR /&gt;PSP_NS = 00000000, PSPLIM_NS = 00000000&lt;BR /&gt;CONTROL_S 00, FAULTMASK_S 00, BASEPRI_S 00, PRIMASK_S 00&lt;BR /&gt;CONTROL_NS 00, FAULTMASK_NS 00, BASEPRI_NS 00, PRIMASK_NS 00&lt;BR /&gt;&lt;BR /&gt;Reading common registers: Read register 'r0' (4 bytes) from hardware: 0x00404020&lt;BR /&gt;Read register 'r1' (4 bytes) from hardware: 0x00000000&lt;BR /&gt;Read register 'r2' (4 bytes) from hardware: 0xEFBEADDE&lt;BR /&gt;Read register 'r3' (4 bytes) from hardware: 0x00044000&lt;BR /&gt;Read register 'r4' (4 bytes) from hardware: 0xB4080020&lt;BR /&gt;Read register 'r5' (4 bytes) from hardware: 0xD4080020&lt;BR /&gt;Read register 'r6' (4 bytes) from hardware: 0xD4080020&lt;BR /&gt;Read register 'r7' (4 bytes) from hardware: 0x00000000&lt;BR /&gt;Read register 'r8' (4 bytes) from hardware: 0x00000000&lt;BR /&gt;Read register 'r9' (4 bytes) from hardware: 0x00000000&lt;BR /&gt;Read register 'r10' (4 bytes) from hardware: 0x00000000&lt;BR /&gt;Read register 'r11' (4 bytes) from hardware: 0x00000000&lt;BR /&gt;Read register 'r12' (4 bytes) from hardware: 0xFE0F0000&lt;BR /&gt;Read register 'sp' (4 bytes) from hardware: 0xA8080020&lt;BR /&gt;Read register 'lr' (4 bytes) from hardware: 0x5B030020&lt;BR /&gt;Read register 'pc' (4 bytes) from hardware: 0x08000020&lt;BR /&gt;Read register 'xpsr' (4 bytes) from hardware: 0x00000061&lt;BR /&gt;Received monitor command: speed 1000&lt;BR /&gt;Target interface speed set to 1000 kHz&lt;BR /&gt;Received monitor command: flash breakpoints 1&lt;BR /&gt;Flash breakpoints enabled&lt;BR /&gt;Received monitor command: semihosting enable&lt;BR /&gt;Semi-hosting enabled (Handle on breakpoint instruction hit)&lt;BR /&gt;Received monitor command: semihosting IOClient 1&lt;BR /&gt;Semihosting I/O set to TELNET Client&lt;BR /&gt;Reading 64 bytes @ address 0x00401600&lt;BR /&gt;Read 2 bytes @ address 0x00401614 (Data = 0xFFFF)&lt;BR /&gt;Received monitor command: clrbp&lt;BR /&gt;Received monitor command: reset&lt;BR /&gt;Resetting target&lt;BR /&gt;Received monitor command: halt&lt;BR /&gt;Halting target CPU...&lt;BR /&gt;...Target halted (PC = 0x20000008)&lt;BR /&gt;Downloading 16192 bytes @ address 0x00400000 - Verified OK&lt;BR /&gt;Downloading 8544 bytes @ address 0x00403F40 - Verified OK&lt;BR /&gt;Downloading 144 bytes @ address 0x004060A0 - Verified OK&lt;BR /&gt;Downloading 1036 bytes @ address 0x00406130 - Verified OK&lt;BR /&gt;Downloading 20 bytes @ address 0x0040653C - Verified OK&lt;BR /&gt;Writing register 'pc' = 0x00401420&lt;BR /&gt;Comparing flash [....................] Done.&lt;BR /&gt;Erasing flash [....................] Done.&lt;BR /&gt;Programming flash [....................] Done.&lt;BR /&gt;Reading 64 bytes @ address 0x00401600&lt;BR /&gt;Read 2 bytes @ address 0x00401614 (Data = 0xFFFF)&lt;BR /&gt;Read 2 bytes @ address 0x00401614 (Data = 0xFFFF)&lt;BR /&gt;Received monitor command: regs&lt;BR /&gt;R0 = 20404000, R1 = 00000000, R2 = DEADBEEF, R3 = 00400400&lt;BR /&gt;R4 = 200008B4, R5 = 200008D4, R6 = 200008D4, R7 = 00000000&lt;BR /&gt;R8 = 00000000, R9 = 00000000, R10= 00000000, R11= 00000000&lt;BR /&gt;R12= 00000FFE, R13= 200008A8, MSP= 200008A8, PSP= 00000000&lt;BR /&gt;R14(LR) = 2000035B, R15(PC) = 20000008&lt;BR /&gt;XPSR 61000000, APSR 60000000, EPSR 01000000, IPSR 00000000&lt;BR /&gt;CFBP 00000000, CONTROL 00, FAULTMASK 00, BASEPRI 00, PRIMASK 00&lt;BR /&gt;&lt;BR /&gt;Security extension regs:&lt;BR /&gt;MSP_S = 00000000, MSPLIM_S = 00000000&lt;BR /&gt;PSP_S = 00000000, PSPLIM_S = 00000000&lt;BR /&gt;MSP_NS = 200008A8, MSPLIM_NS = 00000000&lt;BR /&gt;PSP_NS = 00000000, PSPLIM_NS = 00000000&lt;BR /&gt;CONTROL_S 00, FAULTMASK_S 00, BASEPRI_S 00, PRIMASK_S 00&lt;BR /&gt;CONTROL_NS 00, FAULTMASK_NS 00, BASEPRI_NS 00, PRIMASK_NS 00&lt;BR /&gt;&lt;BR /&gt;Reading common registers: Read register 'r0' (4 bytes) from hardware: 0x00404020&lt;BR /&gt;Read register 'r1' (4 bytes) from hardware: 0x00000000&lt;BR /&gt;Read register 'r2' (4 bytes) from hardware: 0xEFBEADDE&lt;BR /&gt;Read register 'r3' (4 bytes) from hardware: 0x00044000&lt;BR /&gt;Read register 'r4' (4 bytes) from hardware: 0xB4080020&lt;BR /&gt;Read register 'r5' (4 bytes) from hardware: 0xD4080020&lt;BR /&gt;Read register 'r6' (4 bytes) from hardware: 0xD4080020&lt;BR /&gt;Read register 'r7' (4 bytes) from hardware: 0x00000000&lt;BR /&gt;Read register 'r8' (4 bytes) from hardware: 0x00000000&lt;BR /&gt;Read register 'r9' (4 bytes) from hardware: 0x00000000&lt;BR /&gt;Read register 'r10' (4 bytes) from hardware: 0x00000000&lt;BR /&gt;Read register 'r11' (4 bytes) from hardware: 0x00000000&lt;BR /&gt;Read register 'r12' (4 bytes) from hardware: 0xFE0F0000&lt;BR /&gt;Read register 'sp' (4 bytes) from hardware: 0xA8080020&lt;BR /&gt;Read register 'lr' (4 bytes) from hardware: 0x5B030020&lt;BR /&gt;Read register 'pc' (4 bytes) from hardware: 0x08000020&lt;BR /&gt;Read register 'xpsr' (4 bytes) from hardware: 0x00000061&lt;BR /&gt;Setting breakpoint @ address 0x00401614, Kind = 2, Type = THUMB, BPHandle = 0x0003&lt;BR /&gt;Starting target CPU...&lt;BR /&gt;Debugger requested to halt target...&lt;BR /&gt;...Target halted (PC = 0x20000008)&lt;BR /&gt;Reading common registers: Read register 'r0' (4 bytes) from hardware: 0x00404020&lt;BR /&gt;Read register 'r1' (4 bytes) from hardware: 0x00000000&lt;BR /&gt;Read register 'r2' (4 bytes) from hardware: 0xEFBEADDE&lt;BR /&gt;Read register 'r3' (4 bytes) from hardware: 0x00044000&lt;BR /&gt;Read register 'r4' (4 bytes) from hardware: 0xB4080020&lt;BR /&gt;Read register 'r5' (4 bytes) from hardware: 0xD4080020&lt;BR /&gt;Read register 'r6' (4 bytes) from hardware: 0xD4080020&lt;BR /&gt;Read register 'r7' (4 bytes) from hardware: 0x00000000&lt;BR /&gt;Read register 'r8' (4 bytes) from hardware: 0x00000000&lt;BR /&gt;Read register 'r9' (4 bytes) from hardware: 0x00000000&lt;BR /&gt;Read register 'r10' (4 bytes) from hardware: 0x00000000&lt;BR /&gt;Read register 'r11' (4 bytes) from hardware: 0x00000000&lt;BR /&gt;Read register 'r12' (4 bytes) from hardware: 0xFE0F0000&lt;BR /&gt;Read register 'sp' (4 bytes) from hardware: 0xA8080020&lt;BR /&gt;Read register 'lr' (4 bytes) from hardware: 0x5B030020&lt;BR /&gt;Read register 'pc' (4 bytes) from hardware: 0x08000020&lt;BR /&gt;Read register 'xpsr' (4 bytes) from hardware: 0x00000061&lt;BR /&gt;Removing breakpoint @ address 0x00401614, Size = 2&lt;BR /&gt;Read 4 bytes @ address 0x20000008 (Data = 0xDEADE7FE)&lt;BR /&gt;Read 2 bytes @ address 0x20000008 (Data = 0xE7FE)&lt;BR /&gt;Read 4 bytes @ address 0x2000035A (Data = 0xBEEFDEAD)&lt;BR /&gt;Read 2 bytes @ address 0x2000035A (Data = 0xDEAD)&lt;BR /&gt;Read 4 bytes @ address 0x2000035A (Data = 0xBEEFDEAD)&lt;BR /&gt;Read 2 bytes @ address 0x2000035A (Data = 0xDEAD)&lt;BR /&gt;Reading 64 bytes @ address 0x20000000&lt;BR /&gt;Reading 64 bytes @ address 0x20000040&lt;BR /&gt;Reading 64 bytes @ address 0x1FFFFFC0&lt;BR /&gt;WARNING: Failed to read memory @ address 0x1FFFFFC0&lt;BR /&gt;WARNING: Failed to read memory @ address 0x1FFFFFE0&lt;BR /&gt;Reading 64 bytes @ address 0x1FFFFFC0</description>
      <pubDate>Thu, 27 Jul 2023 10:01:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Siul2-Dio-Ip-Example-S32K312/m-p/1694083#M25512</guid>
      <dc:creator>Lita</dc:creator>
      <dc:date>2023-07-27T10:01:23Z</dc:date>
    </item>
    <item>
      <title>Re: Siul2_Dio_Ip_Example_S32K312</title>
      <link>https://community.nxp.com/t5/S32K/Siul2-Dio-Ip-Example-S32K312/m-p/1694799#M25558</link>
      <description>The example appear same error</description>
      <pubDate>Fri, 28 Jul 2023 07:32:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Siul2-Dio-Ip-Example-S32K312/m-p/1694799#M25558</guid>
      <dc:creator>Lita</dc:creator>
      <dc:date>2023-07-28T07:32:18Z</dc:date>
    </item>
    <item>
      <title>Re: Siul2_Dio_Ip_Example_S32K312</title>
      <link>https://community.nxp.com/t5/S32K/Siul2-Dio-Ip-Example-S32K312/m-p/1694861#M25560</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/217547"&gt;@Lita&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Can you try this solution to mass erase the S32K312 project before it is programmed again?&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-SDK/failed-to-power-up-dap-after-program-s32k312-with-pll0-equal/td-p/1609010" target="_blank"&gt;https://community.nxp.com/t5/S32-SDK/failed-to-power-up-dap-after-program-s32k312-with-pll0-equal/td-p/1609010&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;</description>
      <pubDate>Fri, 28 Jul 2023 08:20:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Siul2-Dio-Ip-Example-S32K312/m-p/1694861#M25560</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2023-07-28T08:20:25Z</dc:date>
    </item>
  </channel>
</rss>