<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How will UART communication be utilized in S32K</title>
    <link>https://community.nxp.com/t5/S32K/How-will-UART-communication-be-utilized/m-p/1693102#M25469</link>
    <description>&lt;P&gt;UART Communication:&lt;BR /&gt;a. How will UART communication be utilized in the wake-up alarm and off-timer functionality? (e.g., user configuration, status reporting, debugging, etc.)&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;b. Are there any specific UART configurations or protocols that need to be considered for communication with external devices or other system components?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;</description>
    <pubDate>Wed, 26 Jul 2023 13:18:50 GMT</pubDate>
    <dc:creator>tzyjty</dc:creator>
    <dc:date>2023-07-26T13:18:50Z</dc:date>
    <item>
      <title>How will UART communication be utilized</title>
      <link>https://community.nxp.com/t5/S32K/How-will-UART-communication-be-utilized/m-p/1693102#M25469</link>
      <description>&lt;P&gt;UART Communication:&lt;BR /&gt;a. How will UART communication be utilized in the wake-up alarm and off-timer functionality? (e.g., user configuration, status reporting, debugging, etc.)&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;b. Are there any specific UART configurations or protocols that need to be considered for communication with external devices or other system components?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;</description>
      <pubDate>Wed, 26 Jul 2023 13:18:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-will-UART-communication-be-utilized/m-p/1693102#M25469</guid>
      <dc:creator>tzyjty</dc:creator>
      <dc:date>2023-07-26T13:18:50Z</dc:date>
    </item>
    <item>
      <title>Re: How will UART communication be utilized</title>
      <link>https://community.nxp.com/t5/S32K/How-will-UART-communication-be-utilized/m-p/1693343#M25478</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/218262"&gt;@tzyjty&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The technology reference manual provides information on the operation of each module, the required configuration, and the specifications for each chip, among other details.&lt;/P&gt;
&lt;P&gt;Additionally, you can consult the examples provided with our software which shows with simple applications the operation of the modules.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;B.R.&lt;/P&gt;
&lt;P&gt;VaneB&lt;/P&gt;</description>
      <pubDate>Wed, 26 Jul 2023 19:45:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-will-UART-communication-be-utilized/m-p/1693343#M25478</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2023-07-26T19:45:12Z</dc:date>
    </item>
  </channel>
</rss>