<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K312 PWM ICU in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K312-PWM-ICU/m-p/1692029#M25400</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Hi NXP Teams，&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;When I capture pwm waveform in icu, using breakpoint running, I capture data is normal, if I directly run full speed and then pause, the captured data is abnormal.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;And interrupt to a flag bit, and then step into the interrupt, the flag bit will be set to 1, direct full speed operation, the flag bit can not be set to 1&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Can you give me some advice? Thanks&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 25 Jul 2023 08:02:20 GMT</pubDate>
    <dc:creator>Zhuang</dc:creator>
    <dc:date>2023-07-25T08:02:20Z</dc:date>
    <item>
      <title>S32K312 PWM ICU</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-PWM-ICU/m-p/1692029#M25400</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi NXP Teams，&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;When I capture pwm waveform in icu, using breakpoint running, I capture data is normal, if I directly run full speed and then pause, the captured data is abnormal.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;And interrupt to a flag bit, and then step into the interrupt, the flag bit will be set to 1, direct full speed operation, the flag bit can not be set to 1&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Can you give me some advice? Thanks&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jul 2023 08:02:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-PWM-ICU/m-p/1692029#M25400</guid>
      <dc:creator>Zhuang</dc:creator>
      <dc:date>2023-07-25T08:02:20Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 PWM ICU</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-PWM-ICU/m-p/1692819#M25443</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/216151"&gt;@Zhuang&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I would need more information.&lt;/P&gt;
&lt;P&gt;Do you use EMIOs and if so, which ICU mode?&lt;/P&gt;
&lt;P&gt;Do you use RTD drivers or your own implementation?&lt;/P&gt;
&lt;P&gt;Can you share the project or a simplified test project that would show the issue, and I could test it on my side?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you,&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 26 Jul 2023 07:48:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-PWM-ICU/m-p/1692819#M25443</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2023-07-26T07:48:13Z</dc:date>
    </item>
  </channel>
</rss>