<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32k144 extended ID issue</title>
    <link>https://community.nxp.com/t5/S32K/S32k144-extended-ID-issue/m-p/786318#M2535</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;from the code I do not see you have IDE bit set for the RX MB.&lt;/P&gt;&lt;P&gt;Refer to the attached example. It sets MB4 to receive extended ID = 0x14440000.&lt;/P&gt;&lt;P&gt;Code was changed to use RX interrupt.&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Nov 2018 12:27:12 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2018-11-28T12:27:12Z</dc:date>
    <item>
      <title>S32k144 extended ID issue</title>
      <link>https://community.nxp.com/t5/S32K/S32k144-extended-ID-issue/m-p/786317#M2534</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="color: #000000;"&gt;i am&amp;nbsp;working on FlexCAN module of S32K144.&amp;nbsp; i am able to transmit and receive CAN frames with standard ID.&amp;nbsp;Here i am facing issue in&amp;nbsp;receiving a CAN frame with extended ID.&lt;/P&gt;&lt;P style="color: #000000;"&gt;I have set IDE bit to 1, still it is not able to receive data.&lt;/P&gt;&lt;P style="color: #000000;"&gt;&lt;/P&gt;&lt;P style="color: #000000;"&gt;Sample code has been attached. please look into it.&lt;/P&gt;&lt;P style="color: #000000;"&gt;&lt;/P&gt;&lt;P style="color: #000000;"&gt;Regards,&lt;/P&gt;&lt;P style="color: #000000;"&gt;Pritam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Nov 2018 12:15:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k144-extended-ID-issue/m-p/786317#M2534</guid>
      <dc:creator>pritampatil</dc:creator>
      <dc:date>2018-11-21T12:15:51Z</dc:date>
    </item>
    <item>
      <title>Re: S32k144 extended ID issue</title>
      <link>https://community.nxp.com/t5/S32K/S32k144-extended-ID-issue/m-p/786318#M2535</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;from the code I do not see you have IDE bit set for the RX MB.&lt;/P&gt;&lt;P&gt;Refer to the attached example. It sets MB4 to receive extended ID = 0x14440000.&lt;/P&gt;&lt;P&gt;Code was changed to use RX interrupt.&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Nov 2018 12:27:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k144-extended-ID-issue/m-p/786318#M2535</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2018-11-28T12:27:12Z</dc:date>
    </item>
  </channel>
</rss>