<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic FTM5 as input capture S32K146 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/FTM5-as-input-capture-S32K146/m-p/785532#M2526</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have configured FTM5 as input capture through PTA29, the configuration structure&amp;nbsp;ftmStatePtr[5] is not stable during the code execution, the values are changing all the time.&amp;nbsp; The other FTM I have configured is FTM1 as pwm generation.&lt;/P&gt;&lt;P&gt;it seems that the address of ftmStatePtr[5] (0x200003ac) is overwritten. The microcontroller I'm using is marked as PS32K146UAVLQ. Did someone find some similar issue?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 21 Sep 2018 07:14:10 GMT</pubDate>
    <dc:creator>eduardplanas</dc:creator>
    <dc:date>2018-09-21T07:14:10Z</dc:date>
    <item>
      <title>FTM5 as input capture S32K146</title>
      <link>https://community.nxp.com/t5/S32K/FTM5-as-input-capture-S32K146/m-p/785532#M2526</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have configured FTM5 as input capture through PTA29, the configuration structure&amp;nbsp;ftmStatePtr[5] is not stable during the code execution, the values are changing all the time.&amp;nbsp; The other FTM I have configured is FTM1 as pwm generation.&lt;/P&gt;&lt;P&gt;it seems that the address of ftmStatePtr[5] (0x200003ac) is overwritten. The microcontroller I'm using is marked as PS32K146UAVLQ. Did someone find some similar issue?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Sep 2018 07:14:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FTM5-as-input-capture-S32K146/m-p/785532#M2526</guid>
      <dc:creator>eduardplanas</dc:creator>
      <dc:date>2018-09-21T07:14:10Z</dc:date>
    </item>
    <item>
      <title>Re: FTM5 as input capture S32K146</title>
      <link>https://community.nxp.com/t5/S32K/FTM5-as-input-capture-S32K146/m-p/785533#M2527</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eduard,&lt;/P&gt;&lt;P&gt;Could you share a test code so that we can test it?&lt;/P&gt;&lt;P&gt;If you don't want to share the code here you may consider creating a ticket.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-329745"&gt;https://community.nxp.com/docs/DOC-329745&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 23 Sep 2018 19:50:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FTM5-as-input-capture-S32K146/m-p/785533#M2527</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2018-09-23T19:50:52Z</dc:date>
    </item>
    <item>
      <title>Re: FTM5 as input capture S32K146</title>
      <link>https://community.nxp.com/t5/S32K/FTM5-as-input-capture-S32K146/m-p/785534#M2528</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eduard,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Based on your description I think these can be the root-causes:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;You try to run different drivers (PWM and Input Capture) on the same instance.&lt;/LI&gt;&lt;LI&gt;You use the same state structure for both drivers initialization.&amp;nbsp;&lt;/LI&gt;&lt;LI&gt;Also, check if the pointers are well sent to init function.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To detect the first 2 cases you can add&amp;nbsp;DEV_ERROR_DETECT define when you&amp;nbsp;compile your project.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Razvan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Sep 2018 08:54:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FTM5-as-input-capture-S32K146/m-p/785534#M2528</guid>
      <dc:creator>razva_tilimpea</dc:creator>
      <dc:date>2018-09-25T08:54:58Z</dc:date>
    </item>
  </channel>
</rss>