<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: adc sdk in S32K</title>
    <link>https://community.nxp.com/t5/S32K/adc-sdk/m-p/1689689#M25236</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/220118"&gt;@siiv&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The SDK includes four examples of ADC:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;ADC Low Power&lt;/LI&gt;
&lt;LI&gt;ADC Hardware Trigger&lt;/LI&gt;
&lt;LI&gt;ADC PAL example&lt;/LI&gt;
&lt;LI&gt;ADC Software Trigger&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Also, there are this two examples that you could use as a reference:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K144-PDB-ADC-trigger-DMA-ISR-S32DS/ta-p/1103221" target="_blank" rel="noopener"&gt;Example S32K144 PDB ADC trigger DMA ISR S32DS&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K144-PDB-ADC-DMA-S32DS-ARM-2018-R1/ta-p/1101686" target="_blank" rel="noopener"&gt;Example S32K144 PDB ADC DMA S32DS.ARM.2018.R1&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;If you do not need to use the SDK, we also have an ADC example in the &lt;A href="https://www.nxp.com/docs/en/application-note/AN5413.pdf" target="_blank" rel="noopener"&gt;S32K1xx Series Cookbook&lt;/A&gt;&amp;nbsp;and the &lt;A href="https://www.nxp.com/docs/en/application-note/AN12217.pdf" target="_blank" rel="noopener"&gt;S32K1xx ADC guidelines, specs, and configuration&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;B.R.&lt;/P&gt;
&lt;P&gt;VaneB&lt;/P&gt;</description>
    <pubDate>Thu, 20 Jul 2023 18:42:00 GMT</pubDate>
    <dc:creator>VaneB</dc:creator>
    <dc:date>2023-07-20T18:42:00Z</dc:date>
    <item>
      <title>adc sdk</title>
      <link>https://community.nxp.com/t5/S32K/adc-sdk/m-p/1689568#M25232</link>
      <description>&lt;P&gt;i want a simple example to read adc values in s32k144 evb using driver apis&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 20 Jul 2023 15:59:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/adc-sdk/m-p/1689568#M25232</guid>
      <dc:creator>siiv</dc:creator>
      <dc:date>2023-07-20T15:59:20Z</dc:date>
    </item>
    <item>
      <title>Re: adc sdk</title>
      <link>https://community.nxp.com/t5/S32K/adc-sdk/m-p/1689689#M25236</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/220118"&gt;@siiv&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The SDK includes four examples of ADC:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;ADC Low Power&lt;/LI&gt;
&lt;LI&gt;ADC Hardware Trigger&lt;/LI&gt;
&lt;LI&gt;ADC PAL example&lt;/LI&gt;
&lt;LI&gt;ADC Software Trigger&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Also, there are this two examples that you could use as a reference:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K144-PDB-ADC-trigger-DMA-ISR-S32DS/ta-p/1103221" target="_blank" rel="noopener"&gt;Example S32K144 PDB ADC trigger DMA ISR S32DS&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K144-PDB-ADC-DMA-S32DS-ARM-2018-R1/ta-p/1101686" target="_blank" rel="noopener"&gt;Example S32K144 PDB ADC DMA S32DS.ARM.2018.R1&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;If you do not need to use the SDK, we also have an ADC example in the &lt;A href="https://www.nxp.com/docs/en/application-note/AN5413.pdf" target="_blank" rel="noopener"&gt;S32K1xx Series Cookbook&lt;/A&gt;&amp;nbsp;and the &lt;A href="https://www.nxp.com/docs/en/application-note/AN12217.pdf" target="_blank" rel="noopener"&gt;S32K1xx ADC guidelines, specs, and configuration&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;B.R.&lt;/P&gt;
&lt;P&gt;VaneB&lt;/P&gt;</description>
      <pubDate>Thu, 20 Jul 2023 18:42:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/adc-sdk/m-p/1689689#M25236</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2023-07-20T18:42:00Z</dc:date>
    </item>
    <item>
      <title>Re: adc sdk</title>
      <link>https://community.nxp.com/t5/S32K/adc-sdk/m-p/1700172#M25812</link>
      <description>&lt;P&gt;i atteched my file below can you tell me the whre i did a mistake in that one.i didnt get the adcvalue(variable name)&lt;/P&gt;</description>
      <pubDate>Mon, 07 Aug 2023 10:29:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/adc-sdk/m-p/1700172#M25812</guid>
      <dc:creator>siiv</dc:creator>
      <dc:date>2023-08-07T10:29:51Z</dc:date>
    </item>
  </channel>
</rss>