<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックPWM not generating for s32k324</title>
    <link>https://community.nxp.com/t5/S32K/PWM-not-generating-for-s32k324/m-p/1686824#M25073</link>
    <description>&lt;P&gt;PWM not generating for s32k324 emios_0 channel 4 and emios_0 channel 5. given settings as below EmiosChMode as EMIOS_PWM_IP_MODE_OPWFMB since we have to get variable period and variable duty and EmiosChCounterBus as EMIOS_PWM_IP_BUS_INTERNAL. in mcl EmiosMclClkDivVal is configured as 2, Channel class as variable.&lt;/P&gt;&lt;P&gt;Registers for emios_0 A4, B4 and A5, B5 are being set as per the configuration, but PWM wave form is not generating&lt;/P&gt;</description>
    <pubDate>Wed, 12 Jul 2023 18:22:21 GMT</pubDate>
    <dc:creator>HBH</dc:creator>
    <dc:date>2023-07-12T18:22:21Z</dc:date>
    <item>
      <title>PWM not generating for s32k324</title>
      <link>https://community.nxp.com/t5/S32K/PWM-not-generating-for-s32k324/m-p/1686824#M25073</link>
      <description>&lt;P&gt;PWM not generating for s32k324 emios_0 channel 4 and emios_0 channel 5. given settings as below EmiosChMode as EMIOS_PWM_IP_MODE_OPWFMB since we have to get variable period and variable duty and EmiosChCounterBus as EMIOS_PWM_IP_BUS_INTERNAL. in mcl EmiosMclClkDivVal is configured as 2, Channel class as variable.&lt;/P&gt;&lt;P&gt;Registers for emios_0 A4, B4 and A5, B5 are being set as per the configuration, but PWM wave form is not generating&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jul 2023 18:22:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/PWM-not-generating-for-s32k324/m-p/1686824#M25073</guid>
      <dc:creator>HBH</dc:creator>
      <dc:date>2023-07-12T18:22:21Z</dc:date>
    </item>
    <item>
      <title>Re: PWM not generating for s32k324</title>
      <link>https://community.nxp.com/t5/S32K/PWM-not-generating-for-s32k324/m-p/1688381#M25145</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;try to check eMIOS register setting in debugger. To know global prescaler and internal prescaler are enabled and channel counter is running. You can also check An, Bn register setting. Sn[UCOUT] indicates the output pin state, so if it is toggling, then most probably your pin setting is not correct.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Fri, 14 Jul 2023 09:43:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/PWM-not-generating-for-s32k324/m-p/1688381#M25145</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2023-07-14T09:43:19Z</dc:date>
    </item>
    <item>
      <title>Re: PWM not generating for s32k324</title>
      <link>https://community.nxp.com/t5/S32K/PWM-not-generating-for-s32k324/m-p/1688409#M25149</link>
      <description>&lt;P&gt;given pwm duty cycle is 50%, Value for register A4 and B4 are being set accordingly. attaching the screen shot for the same.&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 14 Jul 2023 10:28:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/PWM-not-generating-for-s32k324/m-p/1688409#M25149</guid>
      <dc:creator>HBH</dc:creator>
      <dc:date>2023-07-14T10:28:18Z</dc:date>
    </item>
    <item>
      <title>Re: PWM not generating for s32k324</title>
      <link>https://community.nxp.com/t5/S32K/PWM-not-generating-for-s32k324/m-p/1688444#M25150</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;this looks normal. Counter seems to be running as flag is set. Mode is OPWMB.&lt;BR /&gt;Do you see UCOUT also change value? What about OUDIS register, if set for channel bit, clear it.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Fri, 14 Jul 2023 10:37:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/PWM-not-generating-for-s32k324/m-p/1688444#M25150</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2023-07-14T10:37:02Z</dc:date>
    </item>
    <item>
      <title>Re: PWM not generating for s32k324</title>
      <link>https://community.nxp.com/t5/S32K/PWM-not-generating-for-s32k324/m-p/1688448#M25151</link>
      <description>&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="HBH_0-1689331206673.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/232472iAD73AF0A5E49CA81/image-size/medium?v=v2&amp;amp;px=400" role="button" title="HBH_0-1689331206673.png" alt="HBH_0-1689331206673.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;the mode i have set is OPWFMB, sharing the updated register snapshot&lt;/P&gt;&lt;P&gt;attaching the screen shot for configuration details also&lt;/P&gt;</description>
      <pubDate>Fri, 14 Jul 2023 12:49:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/PWM-not-generating-for-s32k324/m-p/1688448#M25151</guid>
      <dc:creator>HBH</dc:creator>
      <dc:date>2023-07-14T12:49:51Z</dc:date>
    </item>
    <item>
      <title>Re: PWM not generating for s32k324</title>
      <link>https://community.nxp.com/t5/S32K/PWM-not-generating-for-s32k324/m-p/1688513#M25161</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;well, UCOUT is toggling, so OPWFMB works normal.&lt;BR /&gt;Then check pin setting and be sure you measure right pin.&lt;BR /&gt;Picture names point to 48, is that GPIO48 (PTB16) pin and so controlled by MSCR48?&lt;BR /&gt;Because in port setting you have PCR value 36 that is PTB4 pin, also configurable for eMIOS_0 ch4.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Fri, 14 Jul 2023 12:33:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/PWM-not-generating-for-s32k324/m-p/1688513#M25161</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2023-07-14T12:33:50Z</dc:date>
    </item>
    <item>
      <title>Re: PWM not generating for s32k324</title>
      <link>https://community.nxp.com/t5/S32K/PWM-not-generating-for-s32k324/m-p/1688534#M25162</link>
      <description>&lt;P&gt;its PTB4 and is controlled by&amp;nbsp;&lt;SPAN&gt;MSCR36 and selected&amp;nbsp;eMIOS_0 ch4 as mode. attaching the snapshot for same&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 14 Jul 2023 12:55:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/PWM-not-generating-for-s32k324/m-p/1688534#M25162</guid>
      <dc:creator>HBH</dc:creator>
      <dc:date>2023-07-14T12:55:25Z</dc:date>
    </item>
  </channel>
</rss>