<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Can MCAL and LLD be used simultaneously？ in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Can-MCAL-and-LLD-be-used-simultaneously/m-p/1686267#M25028</link>
    <description>&lt;P&gt;Hi，&lt;/P&gt;&lt;P&gt;Can I use the components in MCAL and LLD simultaneously in S32DS？&lt;/P&gt;</description>
    <pubDate>Wed, 12 Jul 2023 06:05:01 GMT</pubDate>
    <dc:creator>Vernon</dc:creator>
    <dc:date>2023-07-12T06:05:01Z</dc:date>
    <item>
      <title>Can MCAL and LLD be used simultaneously？</title>
      <link>https://community.nxp.com/t5/S32K/Can-MCAL-and-LLD-be-used-simultaneously/m-p/1686267#M25028</link>
      <description>&lt;P&gt;Hi，&lt;/P&gt;&lt;P&gt;Can I use the components in MCAL and LLD simultaneously in S32DS？&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jul 2023 06:05:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-MCAL-and-LLD-be-used-simultaneously/m-p/1686267#M25028</guid>
      <dc:creator>Vernon</dc:creator>
      <dc:date>2023-07-12T06:05:01Z</dc:date>
    </item>
    <item>
      <title>Re: Can MCAL and LLD be used simultaneously？</title>
      <link>https://community.nxp.com/t5/S32K/Can-MCAL-and-LLD-be-used-simultaneously/m-p/1686596#M25057</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/220279"&gt;@Vernon&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes, you can use the components in MCAL (Microcontroller Abstraction Layer) and LLD (Low-Level Drivers) simultaneously in S32DS (S32 Design Studio). However, there are a few things to keep in mind.&lt;/P&gt;&lt;P&gt;MCAL is a higher-level software module that provides a standardized interface to the underlying hardware. It's designed to be portable and reusable across different microcontroller platforms. On the other hand, LLD is a lower-level software module that provides direct access to the hardware. It's typically specific to a particular microcontroller platform.&lt;/P&gt;&lt;P&gt;When using MCAL and LLD together, you need to ensure that there are no conflicts between the two. For example, if both MCAL and LLD are trying to control the same hardware resource, this could lead to unexpected behavior. Therefore, it's important to carefully manage the use of hardware resources when using MCAL and LLD together.&lt;/P&gt;&lt;P&gt;Also, keep in mind that MCAL and LLD may have different software requirements. For example, MCAL typically requires a Real-Time Operating System (RTOS), while LLD may not. Therefore, you need to ensure that your system meets the requirements of both MCAL and LLD.&lt;/P&gt;&lt;P&gt;Finally, while it's technically possible to use MCAL and LLD together, it may not always be the best approach. Depending on your specific needs, it may be more efficient to use either MCAL or LLD, but not both. Therefore, it's important to carefully consider your specific needs and constraints before deciding to use MCAL and LLD together.&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jul 2023 11:31:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-MCAL-and-LLD-be-used-simultaneously/m-p/1686596#M25057</guid>
      <dc:creator>prakashram72</dc:creator>
      <dc:date>2023-07-12T11:31:13Z</dc:date>
    </item>
    <item>
      <title>Re: Can MCAL and LLD be used simultaneously？</title>
      <link>https://community.nxp.com/t5/S32K/Can-MCAL-and-LLD-be-used-simultaneously/m-p/1686946#M25077</link>
      <description>Hi,@prakashram72&lt;BR /&gt;I have benefited a lot, thank you very much.</description>
      <pubDate>Thu, 13 Jul 2023 00:46:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-MCAL-and-LLD-be-used-simultaneously/m-p/1686946#M25077</guid>
      <dc:creator>Vernon</dc:creator>
      <dc:date>2023-07-13T00:46:43Z</dc:date>
    </item>
  </channel>
</rss>