<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 S32K312</title>
    <link>https://community.nxp.com/t5/S32K/S32K312/m-p/1683744#M24878</link>
    <description>&lt;P&gt;我现在在使用S32K312开发，在使用DMA时遇到一些问题：&lt;/P&gt;&lt;P&gt;DMA在正常传输数据，但当我修改DMA源地址数据时，传输到目的地址的数据依旧是原先的值。&lt;/P&gt;&lt;P&gt;但是我发现在我改变DMA源地址数据后手动调用sys_m7_cache_clean()后，传输到目的地址的数据是更新值。&lt;/P&gt;&lt;P&gt;我想知道是不是我的工程有什么地方配置需要调整。&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I am currently developing with S32K312 and am having some problems with DMA:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;DMA is transmitting data normally, but when I modify the DMA source address data, the data transferred to the destination address is still the original value.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;But I found that after I manually called sys_m7_cache_clean() after changing the DMA source address data, the data transferred to the destination address was the updated value.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I would like to know if there is any configuration of my project that needs to be adjusted.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 07 Jul 2023 07:45:45 GMT</pubDate>
    <dc:creator>MUXU</dc:creator>
    <dc:date>2023-07-07T07:45:45Z</dc:date>
    <item>
      <title>S32K312</title>
      <link>https://community.nxp.com/t5/S32K/S32K312/m-p/1683744#M24878</link>
      <description>&lt;P&gt;我现在在使用S32K312开发，在使用DMA时遇到一些问题：&lt;/P&gt;&lt;P&gt;DMA在正常传输数据，但当我修改DMA源地址数据时，传输到目的地址的数据依旧是原先的值。&lt;/P&gt;&lt;P&gt;但是我发现在我改变DMA源地址数据后手动调用sys_m7_cache_clean()后，传输到目的地址的数据是更新值。&lt;/P&gt;&lt;P&gt;我想知道是不是我的工程有什么地方配置需要调整。&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I am currently developing with S32K312 and am having some problems with DMA:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;DMA is transmitting data normally, but when I modify the DMA source address data, the data transferred to the destination address is still the original value.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;But I found that after I manually called sys_m7_cache_clean() after changing the DMA source address data, the data transferred to the destination address was the updated value.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I would like to know if there is any configuration of my project that needs to be adjusted.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 07 Jul 2023 07:45:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312/m-p/1683744#M24878</guid>
      <dc:creator>MUXU</dc:creator>
      <dc:date>2023-07-07T07:45:45Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312</title>
      <link>https://community.nxp.com/t5/S32K/S32K312/m-p/1684958#M24942</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;refer to&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32-SDK/S32K312/m-p/1684957#M3191" target="_blank"&gt;https://community.nxp.com/t5/S32-SDK/S32K312/m-p/1684957#M3191&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Mon, 10 Jul 2023 14:14:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312/m-p/1684958#M24942</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2023-07-10T14:14:22Z</dc:date>
    </item>
  </channel>
</rss>