<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: debug K344 with DP83848YB/NOPB</title>
    <link>https://community.nxp.com/t5/S32K/debug-K344-with-DP83848YB-NOPB/m-p/1682977#M24842</link>
    <description>&lt;P&gt;OK thanks.&lt;SPAN&gt;Do you have any example code available that supports the MII interface? If I intend to use the MII interface, please tell me what configurations should be modified in the lwip_s32k344 example code?&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 06 Jul 2023 08:38:54 GMT</pubDate>
    <dc:creator>wangjunxiao</dc:creator>
    <dc:date>2023-07-06T08:38:54Z</dc:date>
    <item>
      <title>debug K344 with DP83848YB/NOPB</title>
      <link>https://community.nxp.com/t5/S32K/debug-K344-with-DP83848YB-NOPB/m-p/1671570#M24104</link>
      <description>&lt;P&gt;hi~I am using the example lwip_s32k344 ,r&lt;SPAN&gt;eferenced the pdf : LWIP_S32K344 DEMO SETUP .&lt;/SPAN&gt;&lt;SPAN&gt;I have made the corresponding configuration according to the next image.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="20230617-192801.jpg" style="width: 656px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/228239i2A0D4A01F6C45828/image-size/large?v=v2&amp;amp;px=999" role="button" title="20230617-192801.jpg" alt="20230617-192801.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;but when i debug the project ,it always in this while loop.&lt;SPAN&gt;What could be the possible reasons? see the picture&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="20230617-192542.jpg" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/228240i6E6185693876875A/image-size/large?v=v2&amp;amp;px=999" role="button" title="20230617-192542.jpg" alt="20230617-192542.jpg" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Additionally，in the pdf&amp;nbsp;LWIP_S32K344 DEMO SETUP there is an important note like:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;- Change the S32K344 EVB J30 jumper from 3-4 to 1-2, thus the VDD_HV_B will be changed to 5V, to enhance the ethernet level-shifter stability at RMII 50MHz&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;However,&amp;nbsp; we provide 3.3V, would there be any trouble?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Finally, I have attached the sample code I debugged myself. Could you please help me identify the reasons behind my continuous debugging failures？&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 19 Jun 2023 03:36:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/debug-K344-with-DP83848YB-NOPB/m-p/1671570#M24104</guid>
      <dc:creator>wangjunxiao</dc:creator>
      <dc:date>2023-06-19T03:36:25Z</dc:date>
    </item>
    <item>
      <title>Re: debug K344 with DP83848YB/NOPB</title>
      <link>https://community.nxp.com/t5/S32K/debug-K344-with-DP83848YB-NOPB/m-p/1674314#M24283</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;could you please specify which boards/revisions you are using?&amp;nbsp;&lt;BR /&gt;As far as I know you should ensure to have the VDD_HV_B/Ethernet level-shifter voltage jumper at 5V. to make example running properly.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR, Petr&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 22 Jun 2023 09:02:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/debug-K344-with-DP83848YB-NOPB/m-p/1674314#M24283</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2023-06-22T09:02:41Z</dc:date>
    </item>
    <item>
      <title>Re: debug K344 with DP83848YB/NOPB</title>
      <link>https://community.nxp.com/t5/S32K/debug-K344-with-DP83848YB-NOPB/m-p/1675346#M24334</link>
      <description>&lt;P&gt;&lt;SPAN&gt;We have designed our own circuit using DP83848YB, and the schematic section is shown in the attached image. We are currently supplying it with 5V and use 50MHZ crystal oscillator, but even after setting it up on the PC side, we are unable to ping the board&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="20230625-124412.jpg" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/229123i2AC22A17907AF853/image-size/large?v=v2&amp;amp;px=999" role="button" title="20230625-124412.jpg" alt="20230625-124412.jpg" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Please help me analyze if there are any other reasons causing the network connection issue. thanks&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sun, 25 Jun 2023 05:07:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/debug-K344-with-DP83848YB-NOPB/m-p/1675346#M24334</guid>
      <dc:creator>wangjunxiao</dc:creator>
      <dc:date>2023-06-25T05:07:01Z</dc:date>
    </item>
    <item>
      <title>Re: debug K344 with DP83848YB/NOPB</title>
      <link>https://community.nxp.com/t5/S32K/debug-K344-with-DP83848YB-NOPB/m-p/1677821#M24525</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;hard to say for custom designed board. You can e.g. try read out PHY registers and check for correct setting and check for status/errors etc.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Wed, 28 Jun 2023 11:03:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/debug-K344-with-DP83848YB-NOPB/m-p/1677821#M24525</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2023-06-28T11:03:12Z</dc:date>
    </item>
    <item>
      <title>Re: debug K344 with DP83848YB/NOPB</title>
      <link>https://community.nxp.com/t5/S32K/debug-K344-with-DP83848YB-NOPB/m-p/1682977#M24842</link>
      <description>&lt;P&gt;OK thanks.&lt;SPAN&gt;Do you have any example code available that supports the MII interface? If I intend to use the MII interface, please tell me what configurations should be modified in the lwip_s32k344 example code?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 06 Jul 2023 08:38:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/debug-K344-with-DP83848YB-NOPB/m-p/1682977#M24842</guid>
      <dc:creator>wangjunxiao</dc:creator>
      <dc:date>2023-07-06T08:38:54Z</dc:date>
    </item>
    <item>
      <title>Re: debug K344 with DP83848YB/NOPB</title>
      <link>https://community.nxp.com/t5/S32K/debug-K344-with-DP83848YB-NOPB/m-p/1683740#M24876</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;attached is some hint doc only.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Fri, 07 Jul 2023 07:39:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/debug-K344-with-DP83848YB-NOPB/m-p/1683740#M24876</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2023-07-07T07:39:01Z</dc:date>
    </item>
    <item>
      <title>Re: debug K344 with DP83848YB/NOPB</title>
      <link>https://community.nxp.com/t5/S32K/debug-K344-with-DP83848YB-NOPB/m-p/1683742#M24877</link>
      <description>&lt;P&gt;thank you for your suppoort&lt;/P&gt;</description>
      <pubDate>Fri, 07 Jul 2023 07:43:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/debug-K344-with-DP83848YB-NOPB/m-p/1683742#M24877</guid>
      <dc:creator>wangjunxiao</dc:creator>
      <dc:date>2023-07-07T07:43:28Z</dc:date>
    </item>
  </channel>
</rss>