<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MCSXTE2BK142 single shunt code can't work in S32K</title>
    <link>https://community.nxp.com/t5/S32K/MCSXTE2BK142-single-shunt-code-can-t-work/m-p/1682864#M24834</link>
    <description>&lt;P&gt;i am not able to run it in dual shunt specifically in closed loop. Have you tried with sensoed or sensor less which type of sensor you have used.&lt;/P&gt;</description>
    <pubDate>Thu, 06 Jul 2023 07:16:06 GMT</pubDate>
    <dc:creator>Shrikant1</dc:creator>
    <dc:date>2023-07-06T07:16:06Z</dc:date>
    <item>
      <title>MCSXTE2BK142 single shunt code can't work</title>
      <link>https://community.nxp.com/t5/S32K/MCSXTE2BK142-single-shunt-code-can-t-work/m-p/1609245#M21115</link>
      <description>MCSXTE2BK142\sw\MCSXTE2BK142_PMSM_FOC_1Sh</description>
      <pubDate>Fri, 03 Mar 2023 13:59:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/MCSXTE2BK142-single-shunt-code-can-t-work/m-p/1609245#M21115</guid>
      <dc:creator>peter_shi</dc:creator>
      <dc:date>2023-03-03T13:59:44Z</dc:date>
    </item>
    <item>
      <title>Re: MCSXTE2BK142 single shunt code can't work</title>
      <link>https://community.nxp.com/t5/S32K/MCSXTE2BK142-single-shunt-code-can-t-work/m-p/1610067#M21156</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/123522"&gt;@peter_shi&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Can you be more specific?&lt;/P&gt;
&lt;P&gt;What error does the FreeMaster report?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;</description>
      <pubDate>Mon, 06 Mar 2023 14:25:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/MCSXTE2BK142-single-shunt-code-can-t-work/m-p/1610067#M21156</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2023-03-06T14:25:45Z</dc:date>
    </item>
    <item>
      <title>Re: MCSXTE2BK142 single shunt code can't work</title>
      <link>https://community.nxp.com/t5/S32K/MCSXTE2BK142-single-shunt-code-can-t-work/m-p/1610847#M21187</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I bought 1 pcs&amp;nbsp;&lt;SPAN&gt;MCSXTE2BK142 demo board from your Website and download the demo code from the website as well.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;When I used the two-shunt resistance, the function is ok. I could run motors.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;For the single-shunt demo code, I removed C68, C70, and C65 to check the function.&amp;nbsp; VF function is ok. But when I used sensor-less control, the motor can't run even if it was in open loop stage.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I checked the demo code about ADC configuration, I found the ADC configuration was wrong. The demo code used CH8, but Hardware used CH15.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I reconfigured the ADC channel, but it still doesn't work. FreeMaster report phase over current. I think dc-current sampling has some issue.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 07 Mar 2023 11:04:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/MCSXTE2BK142-single-shunt-code-can-t-work/m-p/1610847#M21187</guid>
      <dc:creator>peter_shi</dc:creator>
      <dc:date>2023-03-07T11:04:10Z</dc:date>
    </item>
    <item>
      <title>Re: MCSXTE2BK142 single shunt code can't work</title>
      <link>https://community.nxp.com/t5/S32K/MCSXTE2BK142-single-shunt-code-can-t-work/m-p/1614755#M21350</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/123522"&gt;@peter_shi&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I'm sorry for the delay.&lt;/P&gt;
&lt;P&gt;It looks like you are right, but the issue is still under investigation.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;</description>
      <pubDate>Tue, 14 Mar 2023 08:39:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/MCSXTE2BK142-single-shunt-code-can-t-work/m-p/1614755#M21350</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2023-03-14T08:39:11Z</dc:date>
    </item>
    <item>
      <title>Re: MCSXTE2BK142 single shunt code can't work</title>
      <link>https://community.nxp.com/t5/S32K/MCSXTE2BK142-single-shunt-code-can-t-work/m-p/1616366#M21413</link>
      <description>&lt;P&gt;Hi Peter,&lt;/P&gt;&lt;P&gt;1. you are right, the ADC channel should be modified to CH15.&lt;/P&gt;&lt;P&gt;2. could you remove the interrupt control&amp;nbsp;&lt;STRONG&gt;INT_SYS_DisableIRQGlobal(); &lt;/STRONG&gt;and&amp;nbsp;&lt;STRONG&gt;INT_SYS_EnableIRQGlobal();&lt;/STRONG&gt;&amp;nbsp;in function&amp;nbsp;&lt;STRONG&gt;ADC0_IRQHandler(). &lt;/STRONG&gt;and try again? I think the FTM3 overflow IRQ routine was delayed by the ADC0 IRQ routine.&lt;/P&gt;</description>
      <pubDate>Thu, 16 Mar 2023 04:19:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/MCSXTE2BK142-single-shunt-code-can-t-work/m-p/1616366#M21413</guid>
      <dc:creator>jianqiuhu</dc:creator>
      <dc:date>2023-03-16T04:19:39Z</dc:date>
    </item>
    <item>
      <title>Re: MCSXTE2BK142 single shunt code can't work</title>
      <link>https://community.nxp.com/t5/S32K/MCSXTE2BK142-single-shunt-code-can-t-work/m-p/1682864#M24834</link>
      <description>&lt;P&gt;i am not able to run it in dual shunt specifically in closed loop. Have you tried with sensoed or sensor less which type of sensor you have used.&lt;/P&gt;</description>
      <pubDate>Thu, 06 Jul 2023 07:16:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/MCSXTE2BK142-single-shunt-code-can-t-work/m-p/1682864#M24834</guid>
      <dc:creator>Shrikant1</dc:creator>
      <dc:date>2023-07-06T07:16:06Z</dc:date>
    </item>
  </channel>
</rss>