<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRecommendation for microcontroller for IEC 61508 application.</title>
    <link>https://community.nxp.com/t5/S32K/Recommendation-for-microcontroller-for-IEC-61508-application/m-p/1678573#M24638</link>
    <description>&lt;P&gt;Dear community Members&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;We are making an CANopen based Safe Inertial Measurement unit . The IMU will provide Roll and Pitch data over CAN. These IMU will be used on Crane to know the position of the boom.&lt;BR /&gt;We are looking for a 32bit ARM microcontroller specifically to achieve IEC 61508 SIL2 for our sensor. Is it possible to achieve with NXP controller. I could only find ISO 26262 product on NXP website.&lt;/P&gt;&lt;P&gt;Please let me know in case you need further information.&lt;/P&gt;&lt;P&gt;Looking forward for your comments.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thank you in advance.&lt;/P&gt;</description>
    <pubDate>Thu, 29 Jun 2023 09:00:32 GMT</pubDate>
    <dc:creator>devendradevgupta</dc:creator>
    <dc:date>2023-06-29T09:00:32Z</dc:date>
    <item>
      <title>Recommendation for microcontroller for IEC 61508 application.</title>
      <link>https://community.nxp.com/t5/S32K/Recommendation-for-microcontroller-for-IEC-61508-application/m-p/1678573#M24638</link>
      <description>&lt;P&gt;Dear community Members&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;We are making an CANopen based Safe Inertial Measurement unit . The IMU will provide Roll and Pitch data over CAN. These IMU will be used on Crane to know the position of the boom.&lt;BR /&gt;We are looking for a 32bit ARM microcontroller specifically to achieve IEC 61508 SIL2 for our sensor. Is it possible to achieve with NXP controller. I could only find ISO 26262 product on NXP website.&lt;/P&gt;&lt;P&gt;Please let me know in case you need further information.&lt;/P&gt;&lt;P&gt;Looking forward for your comments.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thank you in advance.&lt;/P&gt;</description>
      <pubDate>Thu, 29 Jun 2023 09:00:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Recommendation-for-microcontroller-for-IEC-61508-application/m-p/1678573#M24638</guid>
      <dc:creator>devendradevgupta</dc:creator>
      <dc:date>2023-06-29T09:00:32Z</dc:date>
    </item>
  </channel>
</rss>