<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic 5V supplies for FS32K148UJT0VLQT RMII Interface? in S32K</title>
    <link>https://community.nxp.com/t5/S32K/5V-supplies-for-FS32K148UJT0VLQT-RMII-Interface/m-p/1678987#M24594</link>
    <description>&lt;P&gt;I am having FS32K148UJT0VLQT on my design.&amp;nbsp; Most of my I/O interfaces are 5V, but RMII interface requires 3.3V.&amp;nbsp; I wonder if I can supply 5V to&amp;nbsp;FS32K148UJT0VLQT and level-shift only the RMII interface signals down to 3.3V.&amp;nbsp; I assume with 5V supplies, the RMII signals will become 5V and I can simply level shift them to 3.3.&amp;nbsp; But I am not sure if the FS32K148UJT0VLQT RMII circuitry can handle 5V internally.&amp;nbsp; Not sure if this is a possible solution?&amp;nbsp; Thanks.&lt;/P&gt;</description>
    <pubDate>Thu, 29 Jun 2023 21:09:11 GMT</pubDate>
    <dc:creator>peter123</dc:creator>
    <dc:date>2023-06-29T21:09:11Z</dc:date>
    <item>
      <title>5V supplies for FS32K148UJT0VLQT RMII Interface?</title>
      <link>https://community.nxp.com/t5/S32K/5V-supplies-for-FS32K148UJT0VLQT-RMII-Interface/m-p/1678987#M24594</link>
      <description>&lt;P&gt;I am having FS32K148UJT0VLQT on my design.&amp;nbsp; Most of my I/O interfaces are 5V, but RMII interface requires 3.3V.&amp;nbsp; I wonder if I can supply 5V to&amp;nbsp;FS32K148UJT0VLQT and level-shift only the RMII interface signals down to 3.3V.&amp;nbsp; I assume with 5V supplies, the RMII signals will become 5V and I can simply level shift them to 3.3.&amp;nbsp; But I am not sure if the FS32K148UJT0VLQT RMII circuitry can handle 5V internally.&amp;nbsp; Not sure if this is a possible solution?&amp;nbsp; Thanks.&lt;/P&gt;</description>
      <pubDate>Thu, 29 Jun 2023 21:09:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/5V-supplies-for-FS32K148UJT0VLQT-RMII-Interface/m-p/1678987#M24594</guid>
      <dc:creator>peter123</dc:creator>
      <dc:date>2023-06-29T21:09:11Z</dc:date>
    </item>
    <item>
      <title>Re: 5V supplies for FS32K148UJT0VLQT RMII Interface?</title>
      <link>https://community.nxp.com/t5/S32K/5V-supplies-for-FS32K148UJT0VLQT-RMII-Interface/m-p/1679544#M24627</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;I think you can refer to the schematic of&amp;nbsp;&lt;A href="https://www.nxp.com/webapp/Download?colCode=S32K148EVB-SCH-29644-RB" target="_self"&gt;S32K148EVB-SCH-29644-RB&lt;/A&gt;,&amp;nbsp;TXB0104 is used.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="S32K148EVB-SCH-29644-RB TXB0104.jpg" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/230297iFF624676132EC2F4/image-size/large?v=v2&amp;amp;px=999" role="button" title="S32K148EVB-SCH-29644-RB TXB0104.jpg" alt="S32K148EVB-SCH-29644-RB TXB0104.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 30 Jun 2023 10:06:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/5V-supplies-for-FS32K148UJT0VLQT-RMII-Interface/m-p/1679544#M24627</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2023-06-30T10:06:16Z</dc:date>
    </item>
    <item>
      <title>Re: 5V supplies for FS32K148UJT0VLQT RMII Interface?</title>
      <link>https://community.nxp.com/t5/S32K/5V-supplies-for-FS32K148UJT0VLQT-RMII-Interface/m-p/1679751#M24639</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/57959"&gt;@Robin_Shen&lt;/a&gt;&amp;nbsp; Thanks so much.&amp;nbsp; NXP Tech Support team is impressive.&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 30 Jun 2023 17:15:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/5V-supplies-for-FS32K148UJT0VLQT-RMII-Interface/m-p/1679751#M24639</guid>
      <dc:creator>peter123</dc:creator>
      <dc:date>2023-06-30T17:15:52Z</dc:date>
    </item>
  </channel>
</rss>