<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: I2C pin configuration in S32K</title>
    <link>https://community.nxp.com/t5/S32K/I2C-pin-configuration/m-p/1678043#M24533</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/219343"&gt;@Jusaira&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The configuration of these signals depends on if it uses I2C in&amp;nbsp;4-wire mode or 2-wire mode.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For&amp;nbsp;SCLS in "4-wire mode, this is the SCLS output pin. If LPI2C master/slave are configured to use separate pins, then this the LPI2C slave SCL pin."&lt;/P&gt;
&lt;P&gt;For&amp;nbsp;SDAS&amp;nbsp; in "4-wire mode, this is the SDAS output pin. If LPI2C master/slave are configured to use&lt;BR /&gt;separate pins, then this the LPI2C slave SDA pin."&lt;/P&gt;
&lt;P&gt;Please look at Chapter 52 (Low Power Inter-Integrated Circuit (LPI2C)) of the&amp;nbsp;S32K1xx Series Reference Manual, Rev. 13, for more information about this module.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;B.R&lt;/P&gt;
&lt;P&gt;VaneB&lt;/P&gt;</description>
    <pubDate>Wed, 28 Jun 2023 18:42:10 GMT</pubDate>
    <dc:creator>VaneB</dc:creator>
    <dc:date>2023-06-28T18:42:10Z</dc:date>
    <item>
      <title>I2C pin configuration</title>
      <link>https://community.nxp.com/t5/S32K/I2C-pin-configuration/m-p/1677601#M24503</link>
      <description>&lt;P&gt;Hi team,&lt;/P&gt;&lt;P&gt;I am working on I2C communication in S32K146 in 2-wire scheme. Is there any possible way to use secondary data and clock pins of I2C (LPI2C0_SCLS(PTA0) and LPI2C0_SDAS(PTA1)) for communication instead of LPI2C_SCL(PTA2) and LPI2C0_SDA(PTA3). Please let me know if there is any software configuration possibility for that.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also please give me inputs on how we configure I2C into 2-wire scheme or 4-wire scheme? Should it be done in software?&lt;/P&gt;</description>
      <pubDate>Wed, 28 Jun 2023 08:12:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/I2C-pin-configuration/m-p/1677601#M24503</guid>
      <dc:creator>Jusaira</dc:creator>
      <dc:date>2023-06-28T08:12:40Z</dc:date>
    </item>
    <item>
      <title>Re: I2C pin configuration</title>
      <link>https://community.nxp.com/t5/S32K/I2C-pin-configuration/m-p/1678043#M24533</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/219343"&gt;@Jusaira&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The configuration of these signals depends on if it uses I2C in&amp;nbsp;4-wire mode or 2-wire mode.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For&amp;nbsp;SCLS in "4-wire mode, this is the SCLS output pin. If LPI2C master/slave are configured to use separate pins, then this the LPI2C slave SCL pin."&lt;/P&gt;
&lt;P&gt;For&amp;nbsp;SDAS&amp;nbsp; in "4-wire mode, this is the SDAS output pin. If LPI2C master/slave are configured to use&lt;BR /&gt;separate pins, then this the LPI2C slave SDA pin."&lt;/P&gt;
&lt;P&gt;Please look at Chapter 52 (Low Power Inter-Integrated Circuit (LPI2C)) of the&amp;nbsp;S32K1xx Series Reference Manual, Rev. 13, for more information about this module.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;B.R&lt;/P&gt;
&lt;P&gt;VaneB&lt;/P&gt;</description>
      <pubDate>Wed, 28 Jun 2023 18:42:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/I2C-pin-configuration/m-p/1678043#M24533</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2023-06-28T18:42:10Z</dc:date>
    </item>
  </channel>
</rss>