<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ADC in S32K</title>
    <link>https://community.nxp.com/t5/S32K/ADC/m-p/1677533#M24496</link>
    <description>&lt;P&gt;Hi &lt;SPAN&gt;Shruthi,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;I mentioned three examples to you in your last question. Please tell me which example are you referring to? So that I can troubleshoot the cause for you on the corresponding S32DS and SDK.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Wed, 28 Jun 2023 06:32:34 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2023-06-28T06:32:34Z</dc:date>
    <item>
      <title>ADC</title>
      <link>https://community.nxp.com/t5/S32K/ADC/m-p/1677439#M24488</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using ADC-0 for 5 channels and ADC-1 for 2 channels&lt;/P&gt;&lt;P&gt;Initially configuring&amp;nbsp;both the ADC and calibrating both the ADC using these functions&lt;/P&gt;&lt;P&gt;ADC_DRV_ConfigConverter()&amp;nbsp; for ADC-0&lt;BR /&gt;ADC_DRV_AutoCalibration()&amp;nbsp;for ADC-0&lt;/P&gt;&lt;P&gt;ADC_DRV_ConfigConverter()&amp;nbsp;for ADC-1&lt;BR /&gt;ADC_DRV_AutoCalibration()&amp;nbsp;for ADC-1&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Later I am triggering(software) and configuring the ADC channels using&amp;nbsp;ADC_DRV_ConfigChan function, then I am waiting for COC flag to be set and reading the ADC raw values&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In this scenario I am only getting proper raw values for ADC0 not for ADC-1&lt;/P&gt;&lt;P&gt;Plese support&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Shruthi&lt;/P&gt;</description>
      <pubDate>Wed, 28 Jun 2023 04:39:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ADC/m-p/1677439#M24488</guid>
      <dc:creator>Shruthi_C</dc:creator>
      <dc:date>2023-06-28T04:39:39Z</dc:date>
    </item>
    <item>
      <title>Re: ADC</title>
      <link>https://community.nxp.com/t5/S32K/ADC/m-p/1677533#M24496</link>
      <description>&lt;P&gt;Hi &lt;SPAN&gt;Shruthi,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;I mentioned three examples to you in your last question. Please tell me which example are you referring to? So that I can troubleshoot the cause for you on the corresponding S32DS and SDK.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 28 Jun 2023 06:32:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ADC/m-p/1677533#M24496</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2023-06-28T06:32:34Z</dc:date>
    </item>
    <item>
      <title>Re: ADC</title>
      <link>https://community.nxp.com/t5/S32K/ADC/m-p/1679551#M24628</link>
      <description>&lt;P&gt;Hi Robin,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The PTB0 and PTB1 pins are by default configured to ADC0 but I was configuring ADC-1 without switch configuration so there was a issue&lt;/P&gt;&lt;P&gt;Now resolved by configuring PTB0, PTB1 to ADC0 Thank you Robin.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Shruthi_C_0-1688119823407.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/230298i85FDC674BB38ED24/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Shruthi_C_0-1688119823407.png" alt="Shruthi_C_0-1688119823407.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Shruthi_C_0-1688119823407.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Shruthi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 30 Jun 2023 10:13:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ADC/m-p/1679551#M24628</guid>
      <dc:creator>Shruthi_C</dc:creator>
      <dc:date>2023-06-30T10:13:06Z</dc:date>
    </item>
  </channel>
</rss>