<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic power cycle needed after flash erase/program in S32K</title>
    <link>https://community.nxp.com/t5/S32K/power-cycle-needed-after-flash-erase-program/m-p/1676284#M24416</link>
    <description>&lt;P&gt;When our code reflashes the data flash memory, often (but not always) it is necessary to power cycle the board before the new data reads correctly.&lt;/P&gt;&lt;P&gt;So, for more details, the flash memory is at address 0x10000000 and we write about 10 bytes into it as configuration data. When configurations are to be changed, we erase that sector and then write the new data there. Frequently, after this, the data at address 0x10000000 continues to read the old values until after a power cycle, at which point it holds the new values.&lt;/P&gt;&lt;P&gt;Is there something that the code can do to flush out these stale values?&lt;/P&gt;</description>
    <pubDate>Mon, 26 Jun 2023 18:13:44 GMT</pubDate>
    <dc:creator>KelvinSmith</dc:creator>
    <dc:date>2023-06-26T18:13:44Z</dc:date>
    <item>
      <title>power cycle needed after flash erase/program</title>
      <link>https://community.nxp.com/t5/S32K/power-cycle-needed-after-flash-erase-program/m-p/1676284#M24416</link>
      <description>&lt;P&gt;When our code reflashes the data flash memory, often (but not always) it is necessary to power cycle the board before the new data reads correctly.&lt;/P&gt;&lt;P&gt;So, for more details, the flash memory is at address 0x10000000 and we write about 10 bytes into it as configuration data. When configurations are to be changed, we erase that sector and then write the new data there. Frequently, after this, the data at address 0x10000000 continues to read the old values until after a power cycle, at which point it holds the new values.&lt;/P&gt;&lt;P&gt;Is there something that the code can do to flush out these stale values?&lt;/P&gt;</description>
      <pubDate>Mon, 26 Jun 2023 18:13:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/power-cycle-needed-after-flash-erase-program/m-p/1676284#M24416</guid>
      <dc:creator>KelvinSmith</dc:creator>
      <dc:date>2023-06-26T18:13:44Z</dc:date>
    </item>
    <item>
      <title>Re: power cycle needed after flash erase/program</title>
      <link>https://community.nxp.com/t5/S32K/power-cycle-needed-after-flash-erase-program/m-p/1676610#M24430</link>
      <description>&lt;P&gt;Could you please specify used device's partnumber? Thanks&lt;/P&gt;</description>
      <pubDate>Tue, 27 Jun 2023 05:57:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/power-cycle-needed-after-flash-erase-program/m-p/1676610#M24430</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2023-06-27T05:57:27Z</dc:date>
    </item>
    <item>
      <title>Re: power cycle needed after flash erase/program</title>
      <link>https://community.nxp.com/t5/S32K/power-cycle-needed-after-flash-erase-program/m-p/1677134#M24473</link>
      <description>&lt;P&gt;This is the S32K146.&lt;/P&gt;</description>
      <pubDate>Tue, 27 Jun 2023 15:44:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/power-cycle-needed-after-flash-erase-program/m-p/1677134#M24473</guid>
      <dc:creator>KelvinSmith</dc:creator>
      <dc:date>2023-06-27T15:44:03Z</dc:date>
    </item>
    <item>
      <title>Re: power cycle needed after flash erase/program</title>
      <link>https://community.nxp.com/t5/S32K/power-cycle-needed-after-flash-erase-program/m-p/1678713#M24573</link>
      <description>&lt;P&gt;Do you have disabled cache before flash programming?&lt;/P&gt;
&lt;P&gt;Pay attention to following thread:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K/S32K144-FLASH-CACHE/m-p/778380" target="_blank"&gt;https://community.nxp.com/t5/S32K/S32K144-FLASH-CACHE/m-p/778380&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 29 Jun 2023 12:25:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/power-cycle-needed-after-flash-erase-program/m-p/1678713#M24573</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2023-06-29T12:25:17Z</dc:date>
    </item>
    <item>
      <title>Re: power cycle needed after flash erase/program</title>
      <link>https://community.nxp.com/t5/S32K/power-cycle-needed-after-flash-erase-program/m-p/1679791#M24643</link>
      <description>Thanks, that appears to have solved the problem.</description>
      <pubDate>Fri, 30 Jun 2023 19:05:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/power-cycle-needed-after-flash-erase-program/m-p/1679791#M24643</guid>
      <dc:creator>KelvinSmith</dc:creator>
      <dc:date>2023-06-30T19:05:06Z</dc:date>
    </item>
  </channel>
</rss>