<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32K358 FreeRTOS using multiple cores</title>
    <link>https://community.nxp.com/t5/S32K/S32K358-FreeRTOS-using-multiple-cores/m-p/1676023#M24401</link>
    <description>&lt;P&gt;Unfortunately, FreeRTOS doesn't support Multi-cores by default. As a result, there would be no FreeRTOS example on S32K3 Also, I am afraid that it would not be simple to have FreeRTOS on each core of S32K3. However, there are some topics in the Internet that customers can refer to. Here is one of these:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://forums.freertos.org/t/freertos-and-dual-core/9922" target="_blank"&gt;https://forums.freertos.org/t/freertos-and-dual-core/9922&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://forums.freertos.org/t/multicore-advice-and-suggestions/7781" target="_blank"&gt;https://forums.freertos.org/t/multicore-advice-and-suggestions/7781&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 26 Jun 2023 12:07:33 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2023-06-26T12:07:33Z</dc:date>
    <item>
      <title>S32K358 FreeRTOS using multiple cores</title>
      <link>https://community.nxp.com/t5/S32K/S32K358-FreeRTOS-using-multiple-cores/m-p/1675521#M24346</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using FreeRTOS example for S32K358 from Design Studio.&lt;/P&gt;&lt;P&gt;Currently I can execute FreeRTOS on S32K358.&amp;nbsp;&lt;/P&gt;&lt;P&gt;How can I use multiple cores in FreeRTOS ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I can see start-up code section,&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;#define CM7_0_ENABLE                (1)
#ifndef CM7_1_ENABLE
    #define CM7_1_ENABLE            (0)
#endif
#ifndef CM7_2_ENABLE
    #define CM7_2_ENABLE            (0)
#endif&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But defining "&lt;SPAN&gt;CM7_2_ENABLE" is not making any difference.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Anything more required to enable execution on multiple cores ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Nandan Chaturbhuj&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 26 Jun 2023 01:39:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K358-FreeRTOS-using-multiple-cores/m-p/1675521#M24346</guid>
      <dc:creator>nandanchaturbhuj</dc:creator>
      <dc:date>2023-06-26T01:39:18Z</dc:date>
    </item>
    <item>
      <title>Re: S32K358 FreeRTOS using multiple cores</title>
      <link>https://community.nxp.com/t5/S32K/S32K358-FreeRTOS-using-multiple-cores/m-p/1676023#M24401</link>
      <description>&lt;P&gt;Unfortunately, FreeRTOS doesn't support Multi-cores by default. As a result, there would be no FreeRTOS example on S32K3 Also, I am afraid that it would not be simple to have FreeRTOS on each core of S32K3. However, there are some topics in the Internet that customers can refer to. Here is one of these:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://forums.freertos.org/t/freertos-and-dual-core/9922" target="_blank"&gt;https://forums.freertos.org/t/freertos-and-dual-core/9922&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://forums.freertos.org/t/multicore-advice-and-suggestions/7781" target="_blank"&gt;https://forums.freertos.org/t/multicore-advice-and-suggestions/7781&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 26 Jun 2023 12:07:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K358-FreeRTOS-using-multiple-cores/m-p/1676023#M24401</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2023-06-26T12:07:33Z</dc:date>
    </item>
  </channel>
</rss>