<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Can I use on-board debugger to debug with MULTI IDE</title>
    <link>https://community.nxp.com/t5/S32K/Can-I-use-on-board-debugger-to-debug-with-MULTI-IDE/m-p/1675643#M24353</link>
    <description>&lt;P&gt;Please help me, experts.&lt;/P&gt;</description>
    <pubDate>Mon, 26 Jun 2023 06:12:35 GMT</pubDate>
    <dc:creator>mrtientv6</dc:creator>
    <dc:date>2023-06-26T06:12:35Z</dc:date>
    <item>
      <title>Can I use on-board debugger to debug with MULTI IDE</title>
      <link>https://community.nxp.com/t5/S32K/Can-I-use-on-board-debugger-to-debug-with-MULTI-IDE/m-p/1675197#M24324</link>
      <description>&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;I'm purchasing&amp;nbsp;s32k3x4evb-t172-evaluation-board (&lt;A href="https://www.nxp.com/design/development-boards/automotive-development-platforms/s32k-mcu-platforms/s32k3x4evb-t172-evaluation-board-for-automotive-general-purpose:S32K3X4EVB-T172" target="_blank"&gt;S32K3X4EVB-T172 Evaluation Board for Automotive General Purpose | NXP Semiconductors&lt;/A&gt;) and our project use MULTI IDE (ghs ide-arm-v-20191 rel.9.19.1 - COMP_Version 2019.1.4)&lt;/P&gt;&lt;P&gt;I concern about the debugger that I can use in our project.&lt;/P&gt;&lt;P&gt;Can I select On-board debugger (only need USB cable) in connection setting in MULTI IDE, or I have to use additional debugger probe (JLink/GHS ...)?&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Tien Tran&lt;/P&gt;</description>
      <pubDate>Sat, 24 Jun 2023 04:14:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-I-use-on-board-debugger-to-debug-with-MULTI-IDE/m-p/1675197#M24324</guid>
      <dc:creator>mrtientv6</dc:creator>
      <dc:date>2023-06-24T04:14:06Z</dc:date>
    </item>
    <item>
      <title>Re: Can I use on-board debugger to debug with MULTI IDE</title>
      <link>https://community.nxp.com/t5/S32K/Can-I-use-on-board-debugger-to-debug-with-MULTI-IDE/m-p/1675643#M24353</link>
      <description>&lt;P&gt;Please help me, experts.&lt;/P&gt;</description>
      <pubDate>Mon, 26 Jun 2023 06:12:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-I-use-on-board-debugger-to-debug-with-MULTI-IDE/m-p/1675643#M24353</guid>
      <dc:creator>mrtientv6</dc:creator>
      <dc:date>2023-06-26T06:12:35Z</dc:date>
    </item>
    <item>
      <title>Re: Can I use on-board debugger to debug with MULTI IDE</title>
      <link>https://community.nxp.com/t5/S32K/Can-I-use-on-board-debugger-to-debug-with-MULTI-IDE/m-p/1676117#M24409</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I am not sure if&amp;nbsp;MULTI IDE support&amp;nbsp;&lt;STRONG&gt;Multilink&lt;/STRONG&gt;, you need to check the manual of it.&lt;/P&gt;
&lt;P&gt;All S32K3 boards are programmed with secured K26 PEMicro embedded multilink firmware, also known as OpenSDA.&lt;/P&gt;
&lt;P&gt;Can you please install the latest &lt;A href="https://www.pemicro.com/downloads/download_file.cfm?download_id=53" target="_self"&gt;&lt;STRONG&gt;PEmicro drivers&lt;/STRONG&gt;&lt;/A&gt; and then run a PEmicro drivers test to ensure that all USB drivers are properly installed.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.pemicro.com/support/downloads_find.cfm" target="_blank"&gt;https://www.pemicro.com/support/downloads_find.cfm&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;After installing the drivers and plugin in this board into USB port, please go to your hardware device manager, expand a Jungo tab and see if the Multilink 2.0 USB device is detected.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 26 Jun 2023 15:09:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-I-use-on-board-debugger-to-debug-with-MULTI-IDE/m-p/1676117#M24409</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2023-06-26T15:09:39Z</dc:date>
    </item>
    <item>
      <title>Re: Can I use on-board debugger to debug with MULTI IDE</title>
      <link>https://community.nxp.com/t5/S32K/Can-I-use-on-board-debugger-to-debug-with-MULTI-IDE/m-p/1678850#M24584</link>
      <description>GHS only suppports Greenhills debug probe(V3 and V4). So we decided to use it.&lt;BR /&gt;Thank you.</description>
      <pubDate>Thu, 29 Jun 2023 16:07:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-I-use-on-board-debugger-to-debug-with-MULTI-IDE/m-p/1678850#M24584</guid>
      <dc:creator>mrtientv6</dc:creator>
      <dc:date>2023-06-29T16:07:31Z</dc:date>
    </item>
  </channel>
</rss>