<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 MCSXTE2BK142</title>
    <link>https://community.nxp.com/t5/S32K/MCSXTE2BK142/m-p/1674165#M24272</link>
    <description>&lt;P&gt;I am current using&amp;nbsp;MCSXTE2BK142 kit and its reference sw for 2 shunt.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Motor runs OK in open loop and halts when shifts to close loop.&lt;/P&gt;&lt;P&gt;Current waveforms from MCAT tool is not sinusoidal. Please refer attachment. Actual current waveform when observed on scope are sinusoidal. ( checked in open loop operation)&lt;/P&gt;&lt;P&gt;i doubt that the current acquisition is not happening at correct time (in mid of PWM when lower mosfets are on, please refer attachment.)&lt;/P&gt;&lt;P&gt;Please support to resolve the issue.&lt;/P&gt;</description>
    <pubDate>Thu, 22 Jun 2023 04:09:19 GMT</pubDate>
    <dc:creator>Shrikant1</dc:creator>
    <dc:date>2023-06-22T04:09:19Z</dc:date>
    <item>
      <title>MCSXTE2BK142</title>
      <link>https://community.nxp.com/t5/S32K/MCSXTE2BK142/m-p/1674165#M24272</link>
      <description>&lt;P&gt;I am current using&amp;nbsp;MCSXTE2BK142 kit and its reference sw for 2 shunt.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Motor runs OK in open loop and halts when shifts to close loop.&lt;/P&gt;&lt;P&gt;Current waveforms from MCAT tool is not sinusoidal. Please refer attachment. Actual current waveform when observed on scope are sinusoidal. ( checked in open loop operation)&lt;/P&gt;&lt;P&gt;i doubt that the current acquisition is not happening at correct time (in mid of PWM when lower mosfets are on, please refer attachment.)&lt;/P&gt;&lt;P&gt;Please support to resolve the issue.&lt;/P&gt;</description>
      <pubDate>Thu, 22 Jun 2023 04:09:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/MCSXTE2BK142/m-p/1674165#M24272</guid>
      <dc:creator>Shrikant1</dc:creator>
      <dc:date>2023-06-22T04:09:19Z</dc:date>
    </item>
    <item>
      <title>Re: MCSXTE2BK142</title>
      <link>https://community.nxp.com/t5/S32K/MCSXTE2BK142/m-p/1674540#M24288</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;i tried to open the link but following page is opened.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/The-NXP-Cup-EMEA/The-Freescale-Cup-Qualification-Event-Casablanca-Morocco/ta-p/1105472" target="_blank"&gt;https://community.nxp.com/t5/The-NXP-Cup-EMEA/The-Freescale-Cup-Qualification-Event-Casablanca-Morocco/ta-p/1105472&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 22 Jun 2023 15:26:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/MCSXTE2BK142/m-p/1674540#M24288</guid>
      <dc:creator>Shrikant1</dc:creator>
      <dc:date>2023-06-22T15:26:23Z</dc:date>
    </item>
    <item>
      <title>Re: MCSXTE2BK142</title>
      <link>https://community.nxp.com/t5/S32K/MCSXTE2BK142/m-p/1674578#M24290</link>
      <description>&lt;P&gt;i am using reference code available on NXP site.Please refer attachment&lt;/P&gt;</description>
      <pubDate>Thu, 22 Jun 2023 16:48:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/MCSXTE2BK142/m-p/1674578#M24290</guid>
      <dc:creator>Shrikant1</dc:creator>
      <dc:date>2023-06-22T16:48:29Z</dc:date>
    </item>
    <item>
      <title>Re: MCSXTE2BK142</title>
      <link>https://community.nxp.com/t5/S32K/MCSXTE2BK142/m-p/1686883#M25075</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;
&lt;P&gt;I have test the example &lt;EM&gt;MCSXTE2BK142_PMSM_FOC_2Sh&lt;/EM&gt; and the motor does not stop in closed loop. I consider that it is possibly a tuning problem with the motor you are using. For that I recommend you consult the app note AN4642. If you are using the motor of MCSPTE1AK144 kit, use the PMSM_appconfig.h from the &lt;EM&gt;MCSPTE1AK144_PMSM_FOC_2Sh&lt;/EM&gt; example.&lt;/P&gt;
&lt;P&gt;Regarding the current acquisition, I see that you are observing the &lt;EM&gt;COCO&lt;/EM&gt; signal of &lt;EM&gt;ADC1&lt;/EM&gt;, but if you check &lt;EM&gt;Figure 12&lt;/EM&gt; (AN12235), &lt;EM&gt;IPHB&lt;/EM&gt; and &lt;EM&gt;UDCBUS&lt;/EM&gt; are being measured with &lt;EM&gt;ADC1&lt;/EM&gt;.&lt;/P&gt;
&lt;P&gt;Hope it helps you.&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jul 2023 21:09:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/MCSXTE2BK142/m-p/1686883#M25075</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2023-07-12T21:09:12Z</dc:date>
    </item>
  </channel>
</rss>