<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32K148 lpuart issues</title>
    <link>https://community.nxp.com/t5/S32K/S32K148-lpuart-issues/m-p/1673395#M24244</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;S32DS for ARM v1.3 is really outdated. It is recommended to install &lt;A href="https://www.nxp.com/design/software/development-software/s32-design-studio-ide/s32-design-studio-for-s32-platform:S32DS-S32PLATFORM" target="_self"&gt;S32DS v3.4&lt;/A&gt;+S32K1 SDK RTM v4.0.3.&lt;BR /&gt;I tested lpuart_echo_s32k148 of SDK v4.0.3 and did not encounter this problem.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Wed, 21 Jun 2023 07:47:39 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2023-06-21T07:47:39Z</dc:date>
    <item>
      <title>S32K148 lpuart issues</title>
      <link>https://community.nxp.com/t5/S32K/S32K148-lpuart-issues/m-p/1673236#M24229</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using a S32K148 q176 with S32 Design Studio for ARM v1.3, I am trying to use lpuart example but when I am debugging it I get stuck in a loop in the assemby on this command:&lt;/P&gt;&lt;P&gt;/* Declare a buffer used to store the received data */&lt;BR /&gt;uint8_t buffer[255] = {0, };&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ehrets_0-1687324282974.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/228668iA869D4C1ABA00D8D/image-dimensions/582x293?v=v2" alt="ehrets_0-1687324282974.png" title="ehrets_0-1687324282974.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I am quite unfamiliar with this and unexperienced so I don t really understand what is going on, there might be some set up issues or things I am totally oblivious about. thanks,&lt;/P&gt;&lt;P&gt;Best regards&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 21 Jun 2023 05:27:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148-lpuart-issues/m-p/1673236#M24229</guid>
      <dc:creator>ehrets</dc:creator>
      <dc:date>2023-06-21T05:27:01Z</dc:date>
    </item>
    <item>
      <title>Re: S32K148 lpuart issues</title>
      <link>https://community.nxp.com/t5/S32K/S32K148-lpuart-issues/m-p/1673395#M24244</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;S32DS for ARM v1.3 is really outdated. It is recommended to install &lt;A href="https://www.nxp.com/design/software/development-software/s32-design-studio-ide/s32-design-studio-for-s32-platform:S32DS-S32PLATFORM" target="_self"&gt;S32DS v3.4&lt;/A&gt;+S32K1 SDK RTM v4.0.3.&lt;BR /&gt;I tested lpuart_echo_s32k148 of SDK v4.0.3 and did not encounter this problem.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 21 Jun 2023 07:47:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148-lpuart-issues/m-p/1673395#M24244</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2023-06-21T07:47:39Z</dc:date>
    </item>
  </channel>
</rss>