<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Using SENT as Triggered SENT using Flex IO peripheral in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Using-SENT-as-Triggered-SENT-using-Flex-IO-peripheral/m-p/1672955#M24208</link>
    <description>&lt;P&gt;Can a FlexIO pin be used as an output to send trigger and then receive SENT frames for S32K344? The example project has it set up for FlexIo Sent Receiver alone. Is it possible to make use of the same to act as an output to send trigger pulses to SENT device&amp;nbsp; and then change it to input to receive the SENT frames?&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 20 Jun 2023 18:29:00 GMT</pubDate>
    <dc:creator>AVargh23</dc:creator>
    <dc:date>2023-06-20T18:29:00Z</dc:date>
    <item>
      <title>Using SENT as Triggered SENT using Flex IO peripheral</title>
      <link>https://community.nxp.com/t5/S32K/Using-SENT-as-Triggered-SENT-using-Flex-IO-peripheral/m-p/1672955#M24208</link>
      <description>&lt;P&gt;Can a FlexIO pin be used as an output to send trigger and then receive SENT frames for S32K344? The example project has it set up for FlexIo Sent Receiver alone. Is it possible to make use of the same to act as an output to send trigger pulses to SENT device&amp;nbsp; and then change it to input to receive the SENT frames?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 20 Jun 2023 18:29:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Using-SENT-as-Triggered-SENT-using-Flex-IO-peripheral/m-p/1672955#M24208</guid>
      <dc:creator>AVargh23</dc:creator>
      <dc:date>2023-06-20T18:29:00Z</dc:date>
    </item>
    <item>
      <title>Re: Using SENT as Triggered SENT using Flex IO peripheral</title>
      <link>https://community.nxp.com/t5/S32K/Using-SENT-as-Triggered-SENT-using-Flex-IO-peripheral/m-p/1674248#M24276</link>
      <description>&lt;P&gt;Hi, it is apparently not possible to do it with FlexIO. Pay attention to following thread:&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-use-FlexIO-configuration-to-SENT-SAE-J2716/m-p/878470" target="_blank"&gt;https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-use-FlexIO-configuration-to-SENT-SAE-J2716/m-p/878470&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 22 Jun 2023 07:20:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Using-SENT-as-Triggered-SENT-using-Flex-IO-peripheral/m-p/1674248#M24276</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2023-06-22T07:20:53Z</dc:date>
    </item>
  </channel>
</rss>