<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Can the S32K118 obtain wakeup source function in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Can-the-S32K118-obtain-wakeup-source-function/m-p/1672694#M24194</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/213999"&gt;@feiyiniu&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Becasue the wakeup source is always an interrupt, a SW flag can set in the ISR.&lt;/P&gt;
&lt;P&gt;It was discussed also here:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K/How-to-identify-which-interrupt-changed-Power-Mode-from-VLPS-to/m-p/882087" target="_blank"&gt;https://community.nxp.com/t5/S32K/How-to-identify-which-interrupt-changed-Power-Mode-from-VLPS-to/m-p/882087&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 20 Jun 2023 11:26:50 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2023-06-20T11:26:50Z</dc:date>
    <item>
      <title>Can the S32K118 obtain wakeup source function</title>
      <link>https://community.nxp.com/t5/S32K/Can-the-S32K118-obtain-wakeup-source-function/m-p/1672374#M24166</link>
      <description>&lt;P&gt;I want to implement different wake-up strategies for different wake-up sources, so I need to obtain the current wake-up source. Is there a register that records the wake-up source.Thanks!&lt;/P&gt;</description>
      <pubDate>Tue, 20 Jun 2023 05:07:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-the-S32K118-obtain-wakeup-source-function/m-p/1672374#M24166</guid>
      <dc:creator>feiyiniu</dc:creator>
      <dc:date>2023-06-20T05:07:24Z</dc:date>
    </item>
    <item>
      <title>Re: Can the S32K118 obtain wakeup source function</title>
      <link>https://community.nxp.com/t5/S32K/Can-the-S32K118-obtain-wakeup-source-function/m-p/1672694#M24194</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/213999"&gt;@feiyiniu&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Becasue the wakeup source is always an interrupt, a SW flag can set in the ISR.&lt;/P&gt;
&lt;P&gt;It was discussed also here:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K/How-to-identify-which-interrupt-changed-Power-Mode-from-VLPS-to/m-p/882087" target="_blank"&gt;https://community.nxp.com/t5/S32K/How-to-identify-which-interrupt-changed-Power-Mode-from-VLPS-to/m-p/882087&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 20 Jun 2023 11:26:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-the-S32K118-obtain-wakeup-source-function/m-p/1672694#M24194</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2023-06-20T11:26:50Z</dc:date>
    </item>
  </channel>
</rss>