<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックFraming error detection while TX in UART</title>
    <link>https://community.nxp.com/t5/S32K/Framing-error-detection-while-TX-in-UART/m-p/1672434#M24178</link>
    <description>&lt;P&gt;MCU - S9KEAZN64AMLC&lt;/P&gt;&lt;P&gt;We have a custom board used in LIN communication(UART based) with LIN transceiver while testing for LIN conformance we noticed one test case in which while TX from MCU the BIt error will be introduced, we need to detect it and generate an error response from MCU but while transmission from MCU, we are not able to see Bit error, in the datasheet it is mentioned that Error can be detected in RX&amp;nbsp; nothing mentioned regarding TX.&lt;/P&gt;&lt;P&gt;Is there any way to detect Framing or Noise errors while TX from MCU?&lt;/P&gt;</description>
    <pubDate>Tue, 20 Jun 2023 07:03:25 GMT</pubDate>
    <dc:creator>Sourdev</dc:creator>
    <dc:date>2023-06-20T07:03:25Z</dc:date>
    <item>
      <title>Framing error detection while TX in UART</title>
      <link>https://community.nxp.com/t5/S32K/Framing-error-detection-while-TX-in-UART/m-p/1672434#M24178</link>
      <description>&lt;P&gt;MCU - S9KEAZN64AMLC&lt;/P&gt;&lt;P&gt;We have a custom board used in LIN communication(UART based) with LIN transceiver while testing for LIN conformance we noticed one test case in which while TX from MCU the BIt error will be introduced, we need to detect it and generate an error response from MCU but while transmission from MCU, we are not able to see Bit error, in the datasheet it is mentioned that Error can be detected in RX&amp;nbsp; nothing mentioned regarding TX.&lt;/P&gt;&lt;P&gt;Is there any way to detect Framing or Noise errors while TX from MCU?&lt;/P&gt;</description>
      <pubDate>Tue, 20 Jun 2023 07:03:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Framing-error-detection-while-TX-in-UART/m-p/1672434#M24178</guid>
      <dc:creator>Sourdev</dc:creator>
      <dc:date>2023-06-20T07:03:25Z</dc:date>
    </item>
  </channel>
</rss>