<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32K Encrypted FlexCAN example</title>
    <link>https://community.nxp.com/t5/S32K/S32K-Encrypted-FlexCAN-example/m-p/778764#M2417</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, it was a power supply issue. Thanks for the pointer!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 25 Jun 2018 13:19:04 GMT</pubDate>
    <dc:creator>bix010</dc:creator>
    <dc:date>2018-06-25T13:19:04Z</dc:date>
    <item>
      <title>S32K Encrypted FlexCAN example</title>
      <link>https://community.nxp.com/t5/S32K/S32K-Encrypted-FlexCAN-example/m-p/778761#M2414</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I just got the &lt;A href="https://community.nxp.com/t5/tag/s32k144evb-q100/tg-p"&gt;#s32k144evb-q100&lt;/A&gt; board, and I'm testing the encrypted flexcan example found in the S32 ARM installation folder.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I followed the instructions in the attached file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I step through and debug, I can see the TX function being called when I press the pushbutton&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But on the RX board, I'm not receiving any messages and the LED is not toggling.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Not sure what I'm doing wrong here. Do I need some special cables to connect the CAN ports? Currently I'm only using 3 wires to connect the CAN_H, CAN_L and Ground. Based on the schematics, think pin3 is not used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Appreciate any help!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jun 2018 13:41:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-Encrypted-FlexCAN-example/m-p/778761#M2414</guid>
      <dc:creator>bix010</dc:creator>
      <dc:date>2018-06-13T13:41:07Z</dc:date>
    </item>
    <item>
      <title>Re: S32K Encrypted FlexCAN example</title>
      <link>https://community.nxp.com/t5/S32K/S32K-Encrypted-FlexCAN-example/m-p/778762#M2415</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Do you supply the boards with 12V? The SBCs need 12V.&lt;/P&gt;&lt;P&gt;Could&amp;nbsp;you measure the bus with a scope? If there is no signal, please measure TX signal between the MCU and the SBC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jun 2018 14:10:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-Encrypted-FlexCAN-example/m-p/778762#M2415</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2018-06-13T14:10:41Z</dc:date>
    </item>
    <item>
      <title>Re: S32K Encrypted FlexCAN example</title>
      <link>https://community.nxp.com/t5/S32K/S32K-Encrypted-FlexCAN-example/m-p/778763#M2416</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Did you configure 1 bord as Master and the other as Slave ? Both Boards need to have external power supply for SBC to work, if you had run previously the SBC example you need to reset the SBC to default state, find instructions in doxy for flexcan example.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Jun 2018 09:49:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-Encrypted-FlexCAN-example/m-p/778763#M2416</guid>
      <dc:creator>alexandrunan</dc:creator>
      <dc:date>2018-06-21T09:49:16Z</dc:date>
    </item>
    <item>
      <title>Re: S32K Encrypted FlexCAN example</title>
      <link>https://community.nxp.com/t5/S32K/S32K-Encrypted-FlexCAN-example/m-p/778764#M2417</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, it was a power supply issue. Thanks for the pointer!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Jun 2018 13:19:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-Encrypted-FlexCAN-example/m-p/778764#M2417</guid>
      <dc:creator>bix010</dc:creator>
      <dc:date>2018-06-25T13:19:04Z</dc:date>
    </item>
  </channel>
</rss>