<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic FLEXCAN_ENCRIPT example in S32K</title>
    <link>https://community.nxp.com/t5/S32K/FLEXCAN-ENCRIPT-example/m-p/778706#M2412</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It's running on s32k144 microcontroller. But I simulated some data on the bus with PCAN it cannot be received by RX message buffer when I debuged it. Received message buffer is always in busy state. I don't know why.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Baute rate is set as 500k for both microcontroller and PCAN. it's implemented on CAN0 and FD is false.&amp;nbsp; Interupt is enabled. All configurations are OK. Connection problem is excluded. But no data exchange occured. I have no idea to do it next. Please help me.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 10 Jan 2018 13:49:49 GMT</pubDate>
    <dc:creator>felixfeng</dc:creator>
    <dc:date>2018-01-10T13:49:49Z</dc:date>
    <item>
      <title>FLEXCAN_ENCRIPT example</title>
      <link>https://community.nxp.com/t5/S32K/FLEXCAN-ENCRIPT-example/m-p/778706#M2412</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It's running on s32k144 microcontroller. But I simulated some data on the bus with PCAN it cannot be received by RX message buffer when I debuged it. Received message buffer is always in busy state. I don't know why.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Baute rate is set as 500k for both microcontroller and PCAN. it's implemented on CAN0 and FD is false.&amp;nbsp; Interupt is enabled. All configurations are OK. Connection problem is excluded. But no data exchange occured. I have no idea to do it next. Please help me.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jan 2018 13:49:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FLEXCAN-ENCRIPT-example/m-p/778706#M2412</guid>
      <dc:creator>felixfeng</dc:creator>
      <dc:date>2018-01-10T13:49:49Z</dc:date>
    </item>
    <item>
      <title>Re: FLEXCAN_ENCRIPT example</title>
      <link>https://community.nxp.com/t5/S32K/FLEXCAN-ENCRIPT-example/m-p/778707#M2413</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The problem is found out that enable pin for transeiver is configured with disabled and pull up in default way. After the configuration of enable pin PTB3 for FLEXCAN_0 can modudule started working.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 13 Jan 2018 12:48:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FLEXCAN-ENCRIPT-example/m-p/778707#M2413</guid>
      <dc:creator>felixfeng</dc:creator>
      <dc:date>2018-01-13T12:48:06Z</dc:date>
    </item>
  </channel>
</rss>