<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: CSEc code yields two different UID's?</title>
    <link>https://community.nxp.com/t5/S32K/CSEc-code-yields-two-different-UID-s/m-p/778475#M2411</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;in mpc5777c manual, the UID's 8 lowest significance bits are set 0.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 19 Dec 2018 05:37:07 GMT</pubDate>
    <dc:creator>tong_zhou</dc:creator>
    <dc:date>2018-12-19T05:37:07Z</dc:date>
    <item>
      <title>CSEc code yields two different UID's?</title>
      <link>https://community.nxp.com/t5/S32K/CSEc-code-yields-two-different-UID-s/m-p/778473#M2409</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to load crypto keys into my S32 using the example project "1_Configure_part_and_Load_keys", but the "GET_UID()" function yields two different results in the example vs my project on the same part (CSE_PRAM-&amp;gt;RAMn[11].DATA_32 is different after the operation, so this seems to be an issue with the example)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The UID generated by the example is different only in the last byte - 21120833 vs&amp;nbsp;21120865 - while the upper 3 integers are identical, as shown in the two screenshots of the debug instances.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Interestingly, the driver function "CSEC_DRV_GetID" yields something totally different than the example.. is the example just incorrect?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have attached screenshots of&amp;nbsp;&lt;/P&gt;&lt;P&gt;UID from the NXP example&lt;/P&gt;&lt;P&gt;{14, 1162432521, 909643814, 21120833}&lt;/P&gt;&lt;P&gt;UID from my project running NXP code&amp;nbsp;&lt;/P&gt;&lt;P&gt;{14, 1162432521, 909643814, 21120865}&lt;/P&gt;&lt;P&gt;UID from the Driver function which returned "STATUS_SUCCESS"&lt;/P&gt;&lt;P&gt;{edit - this output is erroneous due to some pointer incompatibility - it's the same as the above in RAM}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is a 0N57U based eval board&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jun 2018 23:15:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CSEc-code-yields-two-different-UID-s/m-p/778473#M2409</guid>
      <dc:creator>gearhead1107</dc:creator>
      <dc:date>2018-06-12T23:15:35Z</dc:date>
    </item>
    <item>
      <title>Re: CSEc code yields two different UID's?</title>
      <link>https://community.nxp.com/t5/S32K/CSEc-code-yields-two-different-UID-s/m-p/778474#M2410</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It looks like the reason the example yields inconsistent results has to do with the fact "UID" is only 15 bytes.&amp;nbsp;&lt;BR /&gt;The example pulls in a full uint32, including the lower 16th byte, while the UID is *only* those upper 15.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If someone from NXP could confirm, it would be appreciated!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jun 2018 00:10:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CSEc-code-yields-two-different-UID-s/m-p/778474#M2410</guid>
      <dc:creator>gearhead1107</dc:creator>
      <dc:date>2018-06-13T00:10:22Z</dc:date>
    </item>
    <item>
      <title>Re: CSEc code yields two different UID's?</title>
      <link>https://community.nxp.com/t5/S32K/CSEc-code-yields-two-different-UID-s/m-p/778475#M2411</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;in mpc5777c manual, the UID's 8 lowest significance bits are set 0.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Dec 2018 05:37:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CSEc-code-yields-two-different-UID-s/m-p/778475#M2411</guid>
      <dc:creator>tong_zhou</dc:creator>
      <dc:date>2018-12-19T05:37:07Z</dc:date>
    </item>
  </channel>
</rss>