<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックLPSPI Clocked Interface feature inquiry !</title>
    <link>https://community.nxp.com/t5/S32K/LPSPI-Clocked-Interface-feature-inquiry/m-p/1671443#M24093</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I need to configure LPSPI "slave" to work in clocked interface mode, datasheet mention that "configure the Peripheral Chip Select Polarity CFGR1[PCSPOL[n]] = 1",but when I do that this feature &lt;STRONG&gt;didn't work&lt;/STRONG&gt; unless set CFGR1[PCSPOL[n]] = 0 !!&lt;/P&gt;&lt;P&gt;another issue about configuring&amp;nbsp; PCS[0] in the pin muxing, should I configure this pin as GPIO input or what ?&lt;/P&gt;</description>
    <pubDate>Sun, 18 Jun 2023 11:11:22 GMT</pubDate>
    <dc:creator>Omar_Megahed</dc:creator>
    <dc:date>2023-06-18T11:11:22Z</dc:date>
    <item>
      <title>LPSPI Clocked Interface feature inquiry !</title>
      <link>https://community.nxp.com/t5/S32K/LPSPI-Clocked-Interface-feature-inquiry/m-p/1671443#M24093</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I need to configure LPSPI "slave" to work in clocked interface mode, datasheet mention that "configure the Peripheral Chip Select Polarity CFGR1[PCSPOL[n]] = 1",but when I do that this feature &lt;STRONG&gt;didn't work&lt;/STRONG&gt; unless set CFGR1[PCSPOL[n]] = 0 !!&lt;/P&gt;&lt;P&gt;another issue about configuring&amp;nbsp; PCS[0] in the pin muxing, should I configure this pin as GPIO input or what ?&lt;/P&gt;</description>
      <pubDate>Sun, 18 Jun 2023 11:11:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LPSPI-Clocked-Interface-feature-inquiry/m-p/1671443#M24093</guid>
      <dc:creator>Omar_Megahed</dc:creator>
      <dc:date>2023-06-18T11:11:22Z</dc:date>
    </item>
    <item>
      <title>Re: LPSPI Clocked Interface feature inquiry !</title>
      <link>https://community.nxp.com/t5/S32K/LPSPI-Clocked-Interface-feature-inquiry/m-p/1672618#M24189</link>
      <description>&lt;P&gt;Could you specify used device? Thanks&lt;/P&gt;</description>
      <pubDate>Tue, 20 Jun 2023 09:45:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LPSPI-Clocked-Interface-feature-inquiry/m-p/1672618#M24189</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2023-06-20T09:45:37Z</dc:date>
    </item>
  </channel>
</rss>