<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: After Reset SRAM Data corruption in S32K</title>
    <link>https://community.nxp.com/t5/S32K/After-Reset-SRAM-Data-corruption/m-p/1671136#M24066</link>
    <description>&lt;P&gt;If you power ON and OFF, data in SRAM dissapeared because it is volatile memory. &lt;/P&gt;
&lt;P&gt;Debugger shows "??????" apparently because you have breakpoint at the very beginning, before SRAM is initialized for ECC. (by 64-bit writes to completely define the ECC code for the data unit)&lt;/P&gt;</description>
    <pubDate>Fri, 16 Jun 2023 12:37:27 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2023-06-16T12:37:27Z</dc:date>
    <item>
      <title>After Reset SRAM Data corruption</title>
      <link>https://community.nxp.com/t5/S32K/After-Reset-SRAM-Data-corruption/m-p/1670316#M24023</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am Using S32K342, in that I am working on Boot Loader, after Flashing application followed by Flash Boot Loader, in normal case could be able to jump to application, but once I power ON and OFF, SRAM data corruption is happening, in Debugger shows "??????", and SRAM init pattern is not initializing so that, ECU is going to hard fault.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Pragadeesh_0-1686834339172.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/227888iA643C3877046D9EA/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Pragadeesh_0-1686834339172.png" alt="Pragadeesh_0-1686834339172.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Pragadeesh_0-1686834339172.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please provide solution for this issue, like where I have to update the code for this issue and which thing I need to modify.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Pragadeesh.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 15 Jun 2023 13:11:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/After-Reset-SRAM-Data-corruption/m-p/1670316#M24023</guid>
      <dc:creator>Pragadeesh</dc:creator>
      <dc:date>2023-06-15T13:11:21Z</dc:date>
    </item>
    <item>
      <title>Re: After Reset SRAM Data corruption</title>
      <link>https://community.nxp.com/t5/S32K/After-Reset-SRAM-Data-corruption/m-p/1671136#M24066</link>
      <description>&lt;P&gt;If you power ON and OFF, data in SRAM dissapeared because it is volatile memory. &lt;/P&gt;
&lt;P&gt;Debugger shows "??????" apparently because you have breakpoint at the very beginning, before SRAM is initialized for ECC. (by 64-bit writes to completely define the ECC code for the data unit)&lt;/P&gt;</description>
      <pubDate>Fri, 16 Jun 2023 12:37:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/After-Reset-SRAM-Data-corruption/m-p/1671136#M24066</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2023-06-16T12:37:27Z</dc:date>
    </item>
  </channel>
</rss>