<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CSECc_MCAL in S32K</title>
    <link>https://community.nxp.com/t5/S32K/CSECc-MCAL/m-p/1670968#M24051</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/218659"&gt;@严雷&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;This is my answer:&lt;/P&gt;
&lt;P&gt;- CRYPTO_KE_FORMAT_BIN_OCTET: format for keys have octal number format - 0x (mostly in use).&lt;BR /&gt;For example:&lt;BR /&gt;static uint8 aKeyPlain[32] = &lt;BR /&gt;{&lt;BR /&gt;0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;0x01, 0x03, 0x53, 0x48, 0x45, 0x00, 0x80, 0x00,&lt;BR /&gt;0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0xb0, &lt;BR /&gt;};&lt;BR /&gt;- CRYPTO_KE_FORMAT_BIN_SHEKEYS: format for keys have SHE key format (least of use).&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Dan&lt;/P&gt;</description>
    <pubDate>Fri, 16 Jun 2023 08:40:14 GMT</pubDate>
    <dc:creator>DanNguyenDuy</dc:creator>
    <dc:date>2023-06-16T08:40:14Z</dc:date>
    <item>
      <title>CSECc_MCAL</title>
      <link>https://community.nxp.com/t5/S32K/CSECc-MCAL/m-p/1667257#M23818</link>
      <description>&lt;P&gt;&lt;SPAN&gt;In the development of S32K information security MCAL, I encountered two parameters of CrytoKeyElementFormat, CRYPTO_KE_FORMAT_BIN_OCTET and CRYPTO_KE_FORMAT_BIN_SHEKEYS, and wanted to ask what is the difference between them.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="屏幕截图 2023-06-11 105058.jpg" style="width: 842px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/227087iC4B12E7BFD9FA70C/image-size/large?v=v2&amp;amp;px=999" role="button" title="屏幕截图 2023-06-11 105058.jpg" alt="屏幕截图 2023-06-11 105058.jpg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;屏幕截图 2023-06-11 105058.jpg&lt;/span&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sun, 11 Jun 2023 02:51:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CSECc-MCAL/m-p/1667257#M23818</guid>
      <dc:creator>严雷</dc:creator>
      <dc:date>2023-06-11T02:51:42Z</dc:date>
    </item>
    <item>
      <title>Re: CSECc_MCAL</title>
      <link>https://community.nxp.com/t5/S32K/CSECc-MCAL/m-p/1670968#M24051</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/218659"&gt;@严雷&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;This is my answer:&lt;/P&gt;
&lt;P&gt;- CRYPTO_KE_FORMAT_BIN_OCTET: format for keys have octal number format - 0x (mostly in use).&lt;BR /&gt;For example:&lt;BR /&gt;static uint8 aKeyPlain[32] = &lt;BR /&gt;{&lt;BR /&gt;0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;0x01, 0x03, 0x53, 0x48, 0x45, 0x00, 0x80, 0x00,&lt;BR /&gt;0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0xb0, &lt;BR /&gt;};&lt;BR /&gt;- CRYPTO_KE_FORMAT_BIN_SHEKEYS: format for keys have SHE key format (least of use).&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Dan&lt;/P&gt;</description>
      <pubDate>Fri, 16 Jun 2023 08:40:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CSECc-MCAL/m-p/1670968#M24051</guid>
      <dc:creator>DanNguyenDuy</dc:creator>
      <dc:date>2023-06-16T08:40:14Z</dc:date>
    </item>
  </channel>
</rss>