<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックFlash Blank Checking</title>
    <link>https://community.nxp.com/t5/S32K/Flash-Blank-Checking/m-p/1670781#M24038</link>
    <description>&lt;P&gt;Hello sirs, I skimmed the reference manual for S32K3XX microcontroller and I can't seem to find a Flash Blank Checking functionality. Can anyone confirm that this is the case? TIA &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 16 Jun 2023 05:40:46 GMT</pubDate>
    <dc:creator>Switcher</dc:creator>
    <dc:date>2023-06-16T05:40:46Z</dc:date>
    <item>
      <title>Flash Blank Checking</title>
      <link>https://community.nxp.com/t5/S32K/Flash-Blank-Checking/m-p/1670781#M24038</link>
      <description>&lt;P&gt;Hello sirs, I skimmed the reference manual for S32K3XX microcontroller and I can't seem to find a Flash Blank Checking functionality. Can anyone confirm that this is the case? TIA &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 16 Jun 2023 05:40:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Flash-Blank-Checking/m-p/1670781#M24038</guid>
      <dc:creator>Switcher</dc:creator>
      <dc:date>2023-06-16T05:40:46Z</dc:date>
    </item>
    <item>
      <title>Re: Flash Blank Checking</title>
      <link>https://community.nxp.com/t5/S32K/Flash-Blank-Checking/m-p/1671191#M24073</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/218979"&gt;@Switcher&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;that's correct, there's no hw blank check functionality. If you check RTD drivers, you can find that C40_Ip_EraseVerify function only reads the flash in a loop and compares if the content is 0xFFFF...&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Fri, 16 Jun 2023 14:59:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Flash-Blank-Checking/m-p/1671191#M24073</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2023-06-16T14:59:36Z</dc:date>
    </item>
    <item>
      <title>Re: Flash Blank Checking</title>
      <link>https://community.nxp.com/t5/S32K/Flash-Blank-Checking/m-p/1671409#M24088</link>
      <description>ty for the reply sir &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;</description>
      <pubDate>Sat, 17 Jun 2023 11:24:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Flash-Blank-Checking/m-p/1671409#M24088</guid>
      <dc:creator>Switcher</dc:creator>
      <dc:date>2023-06-17T11:24:47Z</dc:date>
    </item>
  </channel>
</rss>