<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Issue in capturing Change Frequency in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Issue-in-capturing-Change-Frequency/m-p/1670288#M24021</link>
    <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;I am working with s32k344 series.&lt;/P&gt;&lt;P&gt;Description :&lt;/P&gt;&lt;P&gt;If i set the frequency 1Khz and set the duty 20 %,40% and 60% the ICU get this duty and it will visible into the debug window. But at the runtime if i change the frequency from 1Khz to 2khz and then again i will set the duty for the same frequency like&amp;nbsp;20 %,40% and 60% that time input capture unit capture the wrong duty cycle.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is their any limitation for input capture unit?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Shrikant K&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 15 Jun 2023 12:27:18 GMT</pubDate>
    <dc:creator>shrikantkoli1995</dc:creator>
    <dc:date>2023-06-15T12:27:18Z</dc:date>
    <item>
      <title>Issue in capturing Change Frequency</title>
      <link>https://community.nxp.com/t5/S32K/Issue-in-capturing-Change-Frequency/m-p/1670288#M24021</link>
      <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;I am working with s32k344 series.&lt;/P&gt;&lt;P&gt;Description :&lt;/P&gt;&lt;P&gt;If i set the frequency 1Khz and set the duty 20 %,40% and 60% the ICU get this duty and it will visible into the debug window. But at the runtime if i change the frequency from 1Khz to 2khz and then again i will set the duty for the same frequency like&amp;nbsp;20 %,40% and 60% that time input capture unit capture the wrong duty cycle.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is their any limitation for input capture unit?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Shrikant K&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 15 Jun 2023 12:27:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Issue-in-capturing-Change-Frequency/m-p/1670288#M24021</guid>
      <dc:creator>shrikantkoli1995</dc:creator>
      <dc:date>2023-06-15T12:27:18Z</dc:date>
    </item>
    <item>
      <title>Re: Issue in capturing Change Frequency</title>
      <link>https://community.nxp.com/t5/S32K/Issue-in-capturing-Change-Frequency/m-p/1670914#M24047</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;there should not be limitation, but check if overflows could not happen on selected counter base. If yes try to modify channel prescaler.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Fri, 16 Jun 2023 07:51:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Issue-in-capturing-Change-Frequency/m-p/1670914#M24047</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2023-06-16T07:51:46Z</dc:date>
    </item>
  </channel>
</rss>