<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32k148 AUTOSAR RTD PortPin Pcr in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32k148-AUTOSAR-RTD-PortPin-Pcr/m-p/1668356#M23892</link>
    <description>&lt;P&gt;Hello, I've followed the following walkthrough about blinking LED in Autosar RTD using the s32k144 q100 board, however my own board is s32k148 q176 and my port for swc clock and jtag is 169 instead of 96.&lt;/P&gt;&lt;P&gt;PortPin Pcr part only allows me to input values between 0-155. Give me the error shown in the image.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Create-a-Blinking-LED-example-project-using-S32K1xx-RTD/ta-p/1471695" target="_blank"&gt;https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Create-a-Blinking-LED-example-project-using-S32K1xx-RTD/ta-p/1471695&lt;/A&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 13 Jun 2023 11:25:47 GMT</pubDate>
    <dc:creator>gediz</dc:creator>
    <dc:date>2023-06-13T11:25:47Z</dc:date>
    <item>
      <title>S32k148 AUTOSAR RTD PortPin Pcr</title>
      <link>https://community.nxp.com/t5/S32K/S32k148-AUTOSAR-RTD-PortPin-Pcr/m-p/1668356#M23892</link>
      <description>&lt;P&gt;Hello, I've followed the following walkthrough about blinking LED in Autosar RTD using the s32k144 q100 board, however my own board is s32k148 q176 and my port for swc clock and jtag is 169 instead of 96.&lt;/P&gt;&lt;P&gt;PortPin Pcr part only allows me to input values between 0-155. Give me the error shown in the image.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Create-a-Blinking-LED-example-project-using-S32K1xx-RTD/ta-p/1471695" target="_blank"&gt;https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Create-a-Blinking-LED-example-project-using-S32K1xx-RTD/ta-p/1471695&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 13 Jun 2023 11:25:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k148-AUTOSAR-RTD-PortPin-Pcr/m-p/1668356#M23892</guid>
      <dc:creator>gediz</dc:creator>
      <dc:date>2023-06-13T11:25:47Z</dc:date>
    </item>
    <item>
      <title>Re: S32k148 AUTOSAR RTD PortPin Pcr</title>
      <link>https://community.nxp.com/t5/S32K/S32k148-AUTOSAR-RTD-PortPin-Pcr/m-p/1668652#M23907</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/218763"&gt;@gediz&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;As you are using the S32K148 EVB, some changes are required.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;At the&amp;nbsp;HOWTO: Create a Blinking LED example project using S32K1xx RTD with AUTOSAR is configured the&amp;nbsp;PTD0 (Blue LED) of the S32K144 EVB, but in the board, you are using this LED is connected to&amp;nbsp;PTE23. This means that at step 16,&amp;nbsp;&lt;SPAN&gt;Dio Port Id should be 4, and&amp;nbsp;Dio Channel Id 23. And at step 17.a&amp;nbsp;PortPin Pcr&amp;nbsp;should be 151.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Please refer to Port_Example_S32K148.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;With these changes, the project will work correctly.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;B.R.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;VaneB&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 13 Jun 2023 22:01:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k148-AUTOSAR-RTD-PortPin-Pcr/m-p/1668652#M23907</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2023-06-13T22:01:24Z</dc:date>
    </item>
  </channel>
</rss>