<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Siul2_Port_Ip_Init &amp;amp; Hi-Z in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Siul2-Port-Ip-Init-amp-Hi-Z/m-p/1668326#M23890</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have configured some ports on S32 DS.&lt;/P&gt;&lt;P&gt;And I know this API&amp;nbsp;Siul2_Port_Ip_Init&amp;nbsp;is used to initialize the ports.&lt;/P&gt;&lt;P&gt;My questioin is, if the ports that I configured on S32 DS are not initialized, are they Hi-Z?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Jetty&lt;/P&gt;</description>
    <pubDate>Tue, 13 Jun 2023 10:24:51 GMT</pubDate>
    <dc:creator>jetty_1012</dc:creator>
    <dc:date>2023-06-13T10:24:51Z</dc:date>
    <item>
      <title>Siul2_Port_Ip_Init &amp; Hi-Z</title>
      <link>https://community.nxp.com/t5/S32K/Siul2-Port-Ip-Init-amp-Hi-Z/m-p/1668326#M23890</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have configured some ports on S32 DS.&lt;/P&gt;&lt;P&gt;And I know this API&amp;nbsp;Siul2_Port_Ip_Init&amp;nbsp;is used to initialize the ports.&lt;/P&gt;&lt;P&gt;My questioin is, if the ports that I configured on S32 DS are not initialized, are they Hi-Z?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Jetty&lt;/P&gt;</description>
      <pubDate>Tue, 13 Jun 2023 10:24:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Siul2-Port-Ip-Init-amp-Hi-Z/m-p/1668326#M23890</guid>
      <dc:creator>jetty_1012</dc:creator>
      <dc:date>2023-06-13T10:24:51Z</dc:date>
    </item>
    <item>
      <title>Re: Siul2_Port_Ip_Init &amp; Hi-Z</title>
      <link>https://community.nxp.com/t5/S32K/Siul2-Port-Ip-Init-amp-Hi-Z/m-p/1669541#M23970</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/218754"&gt;@jetty_1012&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;When you don't configure a pin, it maintains the same state it has after a power-up.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please refer to section&amp;nbsp;4.5 (Pin States) of the&amp;nbsp;S32K3xx Reference Manual, Rev. 6.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;B.R.&lt;/P&gt;
&lt;P&gt;VaneB&lt;/P&gt;</description>
      <pubDate>Wed, 14 Jun 2023 18:41:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Siul2-Port-Ip-Init-amp-Hi-Z/m-p/1669541#M23970</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2023-06-14T18:41:23Z</dc:date>
    </item>
  </channel>
</rss>