<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Pull-Up Resistor at GPIO Pin in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Pull-Up-Resistor-at-GPIO-Pin/m-p/1664261#M23673</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using&amp;nbsp;&lt;SPAN&gt;&lt;SPAN class=""&gt;FS32K148UJT0VLUT Controller in my Project. The GPIO current drive is 20mA and less than that.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;In one of the application we require a current drive of more than 20mA (around 50mA max). So, we thought of adding the external pull up resistor at the end of the GPIO pin which will give the more current drive to the DUT in use.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;So, I wanted to know if we can add the pull up resistor at the end of the Push Pull or Open drain transistors.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;The idea behind the current drive is added in the attachments, please do reply to the query asap.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;Regards&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 06 Jun 2023 10:54:26 GMT</pubDate>
    <dc:creator>rak14</dc:creator>
    <dc:date>2023-06-06T10:54:26Z</dc:date>
    <item>
      <title>Pull-Up Resistor at GPIO Pin</title>
      <link>https://community.nxp.com/t5/S32K/Pull-Up-Resistor-at-GPIO-Pin/m-p/1664261#M23673</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using&amp;nbsp;&lt;SPAN&gt;&lt;SPAN class=""&gt;FS32K148UJT0VLUT Controller in my Project. The GPIO current drive is 20mA and less than that.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;In one of the application we require a current drive of more than 20mA (around 50mA max). So, we thought of adding the external pull up resistor at the end of the GPIO pin which will give the more current drive to the DUT in use.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;So, I wanted to know if we can add the pull up resistor at the end of the Push Pull or Open drain transistors.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;The idea behind the current drive is added in the attachments, please do reply to the query asap.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;Regards&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 06 Jun 2023 10:54:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Pull-Up-Resistor-at-GPIO-Pin/m-p/1664261#M23673</guid>
      <dc:creator>rak14</dc:creator>
      <dc:date>2023-06-06T10:54:26Z</dc:date>
    </item>
    <item>
      <title>Re: Pull-Up Resistor at GPIO Pin</title>
      <link>https://community.nxp.com/t5/S32K/Pull-Up-Resistor-at-GPIO-Pin/m-p/1665474#M23723</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;
&lt;P&gt;Feel free to use any device to amplify or switch electrical signals and power but please make sure you are within the spec. For more details, see sections &lt;EM&gt;5.3&lt;/EM&gt; or &lt;EM&gt;5.4&lt;/EM&gt; of the datasheet.&lt;/P&gt;
&lt;P&gt;Hope it helps you.&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;</description>
      <pubDate>Wed, 07 Jun 2023 20:21:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Pull-Up-Resistor-at-GPIO-Pin/m-p/1665474#M23723</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2023-06-07T20:21:00Z</dc:date>
    </item>
  </channel>
</rss>