<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic register MCM_PID in user task in S32K</title>
    <link>https://community.nxp.com/t5/S32K/register-MCM-PID-in-user-task/m-p/1663772#M23634</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I want to use PID to define different access rights for different user tasks. It seems that I should dynamicly change the MCM_PID reigster.&lt;/P&gt;&lt;P&gt;Referring to the RM for S32K1xx, it says the&amp;nbsp;MCM_PID is accessible only in Supervisor mode. While the user tasks are running at user mode. How can I change the MCM_PID in user tasks?&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Yellen&lt;/P&gt;</description>
    <pubDate>Tue, 06 Jun 2023 01:46:13 GMT</pubDate>
    <dc:creator>Yellen</dc:creator>
    <dc:date>2023-06-06T01:46:13Z</dc:date>
    <item>
      <title>register MCM_PID in user task</title>
      <link>https://community.nxp.com/t5/S32K/register-MCM-PID-in-user-task/m-p/1663772#M23634</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I want to use PID to define different access rights for different user tasks. It seems that I should dynamicly change the MCM_PID reigster.&lt;/P&gt;&lt;P&gt;Referring to the RM for S32K1xx, it says the&amp;nbsp;MCM_PID is accessible only in Supervisor mode. While the user tasks are running at user mode. How can I change the MCM_PID in user tasks?&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Yellen&lt;/P&gt;</description>
      <pubDate>Tue, 06 Jun 2023 01:46:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/register-MCM-PID-in-user-task/m-p/1663772#M23634</guid>
      <dc:creator>Yellen</dc:creator>
      <dc:date>2023-06-06T01:46:13Z</dc:date>
    </item>
    <item>
      <title>Re: register MCM_PID in user task</title>
      <link>https://community.nxp.com/t5/S32K/register-MCM-PID-in-user-task/m-p/1668246#M23880</link>
      <description>&lt;P&gt;Could you clarify where it is stated that MCM_PID can be accesses only in supervisor mode? In my opinion it is accessed in both modes.&lt;/P&gt;</description>
      <pubDate>Tue, 13 Jun 2023 09:13:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/register-MCM-PID-in-user-task/m-p/1668246#M23880</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2023-06-13T09:13:39Z</dc:date>
    </item>
    <item>
      <title>Re: register MCM_PID in user task</title>
      <link>https://community.nxp.com/t5/S32K/register-MCM-PID-in-user-task/m-p/1668280#M23885</link>
      <description>&lt;P&gt;Hi David,&lt;/P&gt;&lt;P&gt;Thanks.&amp;nbsp;&lt;/P&gt;&lt;P&gt;It lies in Section 10.3 of&amp;nbsp;S32K1xx Series Reference Manual, Rev. 12.1, 02/2020.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Snipaste_2023-06-13_17-38-20.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/227390i9A03342C3E0D909F/image-size/large?v=v2&amp;amp;px=999" role="button" title="Snipaste_2023-06-13_17-38-20.png" alt="Snipaste_2023-06-13_17-38-20.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Snipaste_2023-06-13_17-38-20.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 13 Jun 2023 09:42:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/register-MCM-PID-in-user-task/m-p/1668280#M23885</guid>
      <dc:creator>Yellen</dc:creator>
      <dc:date>2023-06-13T09:42:54Z</dc:date>
    </item>
    <item>
      <title>Re: register MCM_PID in user task</title>
      <link>https://community.nxp.com/t5/S32K/register-MCM-PID-in-user-task/m-p/1672742#M24200</link>
      <description>&lt;P&gt;I have been confirmed that if application is in user mode, it can not change MCM_PID. Usually, the value of MCM_PID should be defined in supervisor mode.&lt;/P&gt;</description>
      <pubDate>Tue, 20 Jun 2023 12:54:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/register-MCM-PID-in-user-task/m-p/1672742#M24200</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2023-06-20T12:54:14Z</dc:date>
    </item>
    <item>
      <title>Re: register MCM_PID in user task</title>
      <link>https://community.nxp.com/t5/S32K/register-MCM-PID-in-user-task/m-p/1673278#M24233</link>
      <description>&lt;P&gt;So will there be a way to define different values of&amp;nbsp;&lt;SPAN&gt;MCM_PID for user application? Like a lib function that could change to&amp;nbsp;supervisor mode and modify the&amp;nbsp;MCM_PID, then return to user mode?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 21 Jun 2023 06:19:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/register-MCM-PID-in-user-task/m-p/1673278#M24233</guid>
      <dc:creator>Yellen</dc:creator>
      <dc:date>2023-06-21T06:19:54Z</dc:date>
    </item>
  </channel>
</rss>