<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: s32k312 CAN FIFO question?</title>
    <link>https://community.nxp.com/t5/S32K/s32k312-CAN-FIFO-question/m-p/1663413#M23611</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;1-2)&amp;nbsp;ERFFEL registers can be written only in Freeze mode; otherwise, the module blocks them. Thus all RX/TX operations are stopped, as module must be in Freeze mode.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;3) as this is about entering/leaving Freeze mode the max time is specified in MCR[FRZACK] description.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
    <pubDate>Mon, 05 Jun 2023 10:25:42 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2023-06-05T10:25:42Z</dc:date>
    <item>
      <title>s32k312 CAN FIFO question?</title>
      <link>https://community.nxp.com/t5/S32K/s32k312-CAN-FIFO-question/m-p/1662394#M23530</link>
      <description>&lt;P&gt;&lt;SPAN&gt;There are three Rx FIFO to be clarified.&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;1. Enhanced Rx FIFO needs to set ID filter elements as the can message matching condition. Can the RX ID filter elements be dynamically modified?&lt;SPAN&gt;(RX can message reception not be stopped)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;2. When modifying the RX ID filter elements, will the current CAN controller stop receiving all RX can messages? Or will only the modified RX ID filter elements be affected?&lt;/P&gt;&lt;P&gt;3. If any RX ID filter element modification need to turn off RX reception and re-config ID filter elements ,then re-start can message reception. Does NXP have execution time data for reference regarding the time it takes to turn off reception to apply new rules and restart RX reception?&lt;/P&gt;</description>
      <pubDate>Fri, 02 Jun 2023 06:08:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k312-CAN-FIFO-question/m-p/1662394#M23530</guid>
      <dc:creator>StephenYeh</dc:creator>
      <dc:date>2023-06-02T06:08:02Z</dc:date>
    </item>
    <item>
      <title>Re: s32k312 CAN FIFO question?</title>
      <link>https://community.nxp.com/t5/S32K/s32k312-CAN-FIFO-question/m-p/1663413#M23611</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;1-2)&amp;nbsp;ERFFEL registers can be written only in Freeze mode; otherwise, the module blocks them. Thus all RX/TX operations are stopped, as module must be in Freeze mode.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;3) as this is about entering/leaving Freeze mode the max time is specified in MCR[FRZACK] description.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Mon, 05 Jun 2023 10:25:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k312-CAN-FIFO-question/m-p/1663413#M23611</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2023-06-05T10:25:42Z</dc:date>
    </item>
    <item>
      <title>Re: s32k312 CAN FIFO question?</title>
      <link>https://community.nxp.com/t5/S32K/s32k312-CAN-FIFO-question/m-p/1664151#M23665</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi Sir,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Would you help us to check with below question?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;1. Our customer mentioned their previous project can support RX CAN message filter dynamically with AutoSar, what process that AutoSar implement RX can message filter dynamically? &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;And how NXP flexcan driver support RX can message filter changed with AutoSar?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;2. &lt;/SPAN&gt;Could we know how other customer handle the RX filter element modification dynamically in Enhanced Rx FIFO on S32K312?&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;3. &lt;/SPAN&gt;Could you share the necessarily sample code for RX filter element reconfiguration? (We need do RX filter element reconfiguration as less steps).&lt;/P&gt;</description>
      <pubDate>Tue, 06 Jun 2023 08:54:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k312-CAN-FIFO-question/m-p/1664151#M23665</guid>
      <dc:creator>StephenYeh</dc:creator>
      <dc:date>2023-06-06T08:54:13Z</dc:date>
    </item>
    <item>
      <title>Re: s32k312 CAN FIFO question?</title>
      <link>https://community.nxp.com/t5/S32K/s32k312-CAN-FIFO-question/m-p/1664980#M23704</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;1) do not know autosar so cannot comment its implementation. Certainly you can change filters but this must be done in Freeze mode, so a term dynamically is questionable as during Freeze other TX/RX process is not running.&lt;/P&gt;&lt;P&gt;2) nothing to add here&lt;/P&gt;&lt;P&gt;3) the procedure in mentioned in the RM chapter 74.3.8 Enhanced RX FIFO.&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Wed, 07 Jun 2023 08:06:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k312-CAN-FIFO-question/m-p/1664980#M23704</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2023-06-07T08:06:02Z</dc:date>
    </item>
  </channel>
</rss>