<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: I2C Master Receive in S32K</title>
    <link>https://community.nxp.com/t5/S32K/I2C-Master-Receive/m-p/1662976#M23581</link>
    <description>&lt;P&gt;Thank you, Robin,&lt;/P&gt;&lt;P&gt;the sensor was detected and I received an ACK.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sat, 03 Jun 2023 13:09:52 GMT</pubDate>
    <dc:creator>DemaQasem</dc:creator>
    <dc:date>2023-06-03T13:09:52Z</dc:date>
    <item>
      <title>I2C Master Receive</title>
      <link>https://community.nxp.com/t5/S32K/I2C-Master-Receive/m-p/1659738#M23401</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;I am implementing an i2c demo example to receive data from a sensor,&lt;BR /&gt;the s32k144 will act as a master and the sensor as a slave,&lt;/P&gt;&lt;P&gt;I tried to use an example code but all I found was Master Transmitter codes,&lt;/P&gt;&lt;P&gt;is there a simple Master Receiver code available?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Dema.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 30 May 2023 09:07:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/I2C-Master-Receive/m-p/1659738#M23401</guid>
      <dc:creator>DemaQasem</dc:creator>
      <dc:date>2023-05-30T09:07:27Z</dc:date>
    </item>
    <item>
      <title>Re: I2C Master Receive</title>
      <link>https://community.nxp.com/t5/S32K/I2C-Master-Receive/m-p/1660263#M23410</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;Dema,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;It looks like you are referring to the S32K144_Project_LPI2C example in AN5413SW.&lt;BR /&gt;Please install S32DS v3.4 + S32K1 SDK RTM v4.0.3, there are several I2C examples for reference.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="S32K1xx SDK RTM v4.0.3 Examples.jpg" style="width: 803px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/225507i603A88DEAD7866FF/image-size/large?v=v2&amp;amp;px=999" role="button" title="S32K1xx SDK RTM v4.0.3 Examples.jpg" alt="S32K1xx SDK RTM v4.0.3 Examples.jpg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;S32K1xx SDK RTM v4.0.3 Examples.jpg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 31 May 2023 00:49:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/I2C-Master-Receive/m-p/1660263#M23410</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2023-05-31T00:49:45Z</dc:date>
    </item>
    <item>
      <title>Re: I2C Master Receive</title>
      <link>https://community.nxp.com/t5/S32K/I2C-Master-Receive/m-p/1662976#M23581</link>
      <description>&lt;P&gt;Thank you, Robin,&lt;/P&gt;&lt;P&gt;the sensor was detected and I received an ACK.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 03 Jun 2023 13:09:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/I2C-Master-Receive/m-p/1662976#M23581</guid>
      <dc:creator>DemaQasem</dc:creator>
      <dc:date>2023-06-03T13:09:52Z</dc:date>
    </item>
  </channel>
</rss>