<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic For new development cycle which version of packages is suggestable by NXP for S32K144 non autosar in S32K</title>
    <link>https://community.nxp.com/t5/S32K/For-new-development-cycle-which-version-of-packages-is/m-p/1661504#M23474</link>
    <description>&lt;P&gt;suggest the correct SDK, GCC tool chain &amp;amp; RTD version for S32K144 to use LIN communication.&lt;/P&gt;&lt;P&gt;1) S32DS 3.4 / 3.5&amp;nbsp;&lt;/P&gt;&lt;P&gt;2) RTD&amp;nbsp;SW32K1_RTD_4_4_1_0_1_D2202 / S32SDK_S32K1XX_RTM_4.0.3&lt;/P&gt;&lt;P&gt;3) LIN Stack 1.0.1 / 1.0.2&lt;/P&gt;&lt;P&gt;4) DRV driver / IP driver&lt;/P&gt;</description>
    <pubDate>Thu, 01 Jun 2023 05:57:12 GMT</pubDate>
    <dc:creator>SivaB</dc:creator>
    <dc:date>2023-06-01T05:57:12Z</dc:date>
    <item>
      <title>For new development cycle which version of packages is suggestable by NXP for S32K144 non autosar</title>
      <link>https://community.nxp.com/t5/S32K/For-new-development-cycle-which-version-of-packages-is/m-p/1661504#M23474</link>
      <description>&lt;P&gt;suggest the correct SDK, GCC tool chain &amp;amp; RTD version for S32K144 to use LIN communication.&lt;/P&gt;&lt;P&gt;1) S32DS 3.4 / 3.5&amp;nbsp;&lt;/P&gt;&lt;P&gt;2) RTD&amp;nbsp;SW32K1_RTD_4_4_1_0_1_D2202 / S32SDK_S32K1XX_RTM_4.0.3&lt;/P&gt;&lt;P&gt;3) LIN Stack 1.0.1 / 1.0.2&lt;/P&gt;&lt;P&gt;4) DRV driver / IP driver&lt;/P&gt;</description>
      <pubDate>Thu, 01 Jun 2023 05:57:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/For-new-development-cycle-which-version-of-packages-is/m-p/1661504#M23474</guid>
      <dc:creator>SivaB</dc:creator>
      <dc:date>2023-06-01T05:57:12Z</dc:date>
    </item>
    <item>
      <title>Re: For new development cycle which version of packages is suggestable by NXP for S32K144 non autosa</title>
      <link>https://community.nxp.com/t5/S32K/For-new-development-cycle-which-version-of-packages-is/m-p/1661550#M23476</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@SivaB" target="_blank"&gt;Hi@SivaB&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Users can understand some differences between RTD and RTM versions from this answer&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K/difference-between-s32k1-sdk-and-s32k1-rtd/m-p/1637711#M22289" target="_self"&gt;https://community.nxp.com/t5/S32K/difference-between-s32k1-sdk-and-s32k1-rtd/m-p/1637711#M22289&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For applications developed by non-autosar, I personally prefer to use the RTM version, because the RTM SDK will be more concise. If you use the RTM SDK version, you can only use S32 DS V3.4, GCC V6.3.1&lt;/P&gt;
&lt;P&gt;Use RTD to develop Non-Autosar applications, you can try to use the latest S32 DS V3.5, please use the same LIN Stack as the RTD version&lt;/P&gt;</description>
      <pubDate>Thu, 01 Jun 2023 06:55:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/For-new-development-cycle-which-version-of-packages-is/m-p/1661550#M23476</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2023-06-01T06:55:53Z</dc:date>
    </item>
  </channel>
</rss>