<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic NXP s32k116 example linkerscript and startup code in S32K</title>
    <link>https://community.nxp.com/t5/S32K/NXP-s32k116-example-linkerscript-and-startup-code/m-p/1660727#M23438</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;I have installed an autosar package "SW32K1_RTD_4.4_1.0.1" and inside each plugin for example&amp;nbsp; "Adc_TS_T40D2M10I1R0" there exists a folder called examples and there is a folder for each s32k derivative&amp;nbsp; &amp;nbsp;s32k118 , s32k144 , s32k144W ..etc. ,&amp;nbsp; the question is why there is no example for s32k116 this package is supposed to support s32k1xx as it was said also there are files configuration files with extension .epd that is for s32k116.&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;My request is that I want an example linker script and startup code for s32k116 , why doesn't it exist in package ? can you provide me with one?&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Mohamed.&lt;/P&gt;</description>
    <pubDate>Wed, 31 May 2023 10:17:30 GMT</pubDate>
    <dc:creator>MohameddRIAD</dc:creator>
    <dc:date>2023-05-31T10:17:30Z</dc:date>
    <item>
      <title>NXP s32k116 example linkerscript and startup code</title>
      <link>https://community.nxp.com/t5/S32K/NXP-s32k116-example-linkerscript-and-startup-code/m-p/1660727#M23438</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;I have installed an autosar package "SW32K1_RTD_4.4_1.0.1" and inside each plugin for example&amp;nbsp; "Adc_TS_T40D2M10I1R0" there exists a folder called examples and there is a folder for each s32k derivative&amp;nbsp; &amp;nbsp;s32k118 , s32k144 , s32k144W ..etc. ,&amp;nbsp; the question is why there is no example for s32k116 this package is supposed to support s32k1xx as it was said also there are files configuration files with extension .epd that is for s32k116.&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;My request is that I want an example linker script and startup code for s32k116 , why doesn't it exist in package ? can you provide me with one?&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Mohamed.&lt;/P&gt;</description>
      <pubDate>Wed, 31 May 2023 10:17:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/NXP-s32k116-example-linkerscript-and-startup-code/m-p/1660727#M23438</guid>
      <dc:creator>MohameddRIAD</dc:creator>
      <dc:date>2023-05-31T10:17:30Z</dc:date>
    </item>
    <item>
      <title>Re: NXP s32k116 example linkerscript and startup code</title>
      <link>https://community.nxp.com/t5/S32K/NXP-s32k116-example-linkerscript-and-startup-code/m-p/1661345#M23463</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@MohaneddRIAD" target="_blank"&gt;Hi@MohameddRIAD&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;I am attching it for your reference.&lt;/P&gt;</description>
      <pubDate>Thu, 01 Jun 2023 01:56:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/NXP-s32k116-example-linkerscript-and-startup-code/m-p/1661345#M23463</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2023-06-01T01:56:43Z</dc:date>
    </item>
    <item>
      <title>Re: NXP s32k116 example linkerscript and startup code</title>
      <link>https://community.nxp.com/t5/S32K/NXP-s32k116-example-linkerscript-and-startup-code/m-p/1661624#M23482</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;Thank you for your swift response , do you happen to have it in .icf extension to be compatible with IAR tool chain ? , also do you have a corresponding startup code with it ?&lt;/P&gt;</description>
      <pubDate>Thu, 01 Jun 2023 08:24:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/NXP-s32k116-example-linkerscript-and-startup-code/m-p/1661624#M23482</guid>
      <dc:creator>MohameddRIAD</dc:creator>
      <dc:date>2023-06-01T08:24:21Z</dc:date>
    </item>
    <item>
      <title>Re: NXP s32k116 example linkerscript and startup code</title>
      <link>https://community.nxp.com/t5/S32K/NXP-s32k116-example-linkerscript-and-startup-code/m-p/1661630#M23483</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@MohaneddRIAD" target="_blank"&gt;Hi@MohameddRIAD&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;please check the attachment,hope it works for you.&lt;/P&gt;</description>
      <pubDate>Thu, 01 Jun 2023 08:31:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/NXP-s32k116-example-linkerscript-and-startup-code/m-p/1661630#M23483</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2023-06-01T08:31:43Z</dc:date>
    </item>
    <item>
      <title>Re: NXP s32k116 example linkerscript and startup code</title>
      <link>https://community.nxp.com/t5/S32K/NXP-s32k116-example-linkerscript-and-startup-code/m-p/1661649#M23485</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thank you for sharing the attachment. I will take a look and let you know if I have any further questions.&lt;/P&gt;&lt;P&gt;Also, would it be possible for you to share the startup code as well?&lt;/P&gt;&lt;P&gt;Thank you again for your help.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Mohamed.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 01 Jun 2023 08:43:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/NXP-s32k116-example-linkerscript-and-startup-code/m-p/1661649#M23485</guid>
      <dc:creator>MohameddRIAD</dc:creator>
      <dc:date>2023-06-01T08:43:49Z</dc:date>
    </item>
    <item>
      <title>Re: NXP s32k116 example linkerscript and startup code</title>
      <link>https://community.nxp.com/t5/S32K/NXP-s32k116-example-linkerscript-and-startup-code/m-p/1661672#M23486</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@MohameddRIAD" target="_blank"&gt;Hi@MohameddRIAD&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;sure,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If you have installed RTD, you can actually find the corresponding link and startup file in the following path&lt;/P&gt;
&lt;P&gt;etc:&lt;/P&gt;
&lt;P&gt;startup&lt;/P&gt;
&lt;P&gt;C:\NXP\S32DS.3.4\S32DS\software\PlatformSDK_S32K1_2022_02\SW32K1_RTD_4_4_1_0_1_D2202\Platform_TS_T40D2M10I1R0\startup\src&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Senlent_0-1685609664051.png" style="width: 663px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/225809i7843DDA96E8DCBAA/image-dimensions/663x136?v=v2" width="663" height="136" role="button" title="Senlent_0-1685609664051.png" alt="Senlent_0-1685609664051.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Senlent_0-1685609664051.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Linker file&lt;/P&gt;
&lt;P&gt;C:\NXP\S32DS.3.4\S32DS\software\PlatformSDK_S32K1_2022_02\SW32K1_RTD_4_4_1_0_1_D2202\Platform_TS_T40D2M10I1R0\build_files\gcc&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 01 Jun 2023 08:56:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/NXP-s32k116-example-linkerscript-and-startup-code/m-p/1661672#M23486</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2023-06-01T08:56:01Z</dc:date>
    </item>
  </channel>
</rss>