<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K344 14-bit ADC Resolution in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K344-14-bit-ADC-Resolution/m-p/1660645#M23429</link>
    <description>&lt;P&gt;I'm working with the S32K344s ADC. The datasheet and specification on the website states a 12-bit resolution, but the ADC peripheral can be set to 14-bit resolution in the CALBISTREG register.&amp;nbsp;&lt;/P&gt;&lt;P&gt;What would the difference between the 14-bit resolution and 12-bit resolution be if the ADC is specified to 12-bit?&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Oskar Johansson&lt;/P&gt;</description>
    <pubDate>Wed, 31 May 2023 08:53:25 GMT</pubDate>
    <dc:creator>oskarjohansson</dc:creator>
    <dc:date>2023-05-31T08:53:25Z</dc:date>
    <item>
      <title>S32K344 14-bit ADC Resolution</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-14-bit-ADC-Resolution/m-p/1660645#M23429</link>
      <description>&lt;P&gt;I'm working with the S32K344s ADC. The datasheet and specification on the website states a 12-bit resolution, but the ADC peripheral can be set to 14-bit resolution in the CALBISTREG register.&amp;nbsp;&lt;/P&gt;&lt;P&gt;What would the difference between the 14-bit resolution and 12-bit resolution be if the ADC is specified to 12-bit?&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Oskar Johansson&lt;/P&gt;</description>
      <pubDate>Wed, 31 May 2023 08:53:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-14-bit-ADC-Resolution/m-p/1660645#M23429</guid>
      <dc:creator>oskarjohansson</dc:creator>
      <dc:date>2023-05-31T08:53:25Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 14-bit ADC Resolution</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-14-bit-ADC-Resolution/m-p/1661591#M23480</link>
      <description>&lt;P&gt;Hello Oscar,&lt;/P&gt;
&lt;P&gt;The ADC has not been specified at the 14-bit resolution, we don't have any measurements for that.&lt;/P&gt;
&lt;P&gt;Even though the TUE should be slightly better at 14bit resolution, because of the lack of data,&amp;nbsp;we can say that If TUE = +/-4 LSB at 12bit, it is +/-16 LSB at 14bit.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Thu, 01 Jun 2023 07:41:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-14-bit-ADC-Resolution/m-p/1661591#M23480</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2023-06-01T07:41:20Z</dc:date>
    </item>
  </channel>
</rss>