<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K312 PLL_LOL Problem in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K312-PLL-LOL-Problem/m-p/1659424#M23382</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160001"&gt;@danielmartynek&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp; Thanks for your reply. CMU is disable and I am sure the reset reason is&amp;nbsp;&lt;SPAN&gt;PLL Loss of Lock. When PLL LOL,MCU will reset. When&amp;nbsp;set&amp;nbsp;DCMRWP3[9] to 1, mcu will not reset while PLL LOL but mcu will stop running. Thus we cannot&amp;nbsp;change the system clock back to FIRC when PLL LOL. We try to replace the&amp;nbsp;Crystal Oscillator with a higher-power one, it seems better.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 30 May 2023 03:08:29 GMT</pubDate>
    <dc:creator>zhengjianfei1</dc:creator>
    <dc:date>2023-05-30T03:08:29Z</dc:date>
    <item>
      <title>S32K312 PLL_LOL Problem</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-PLL-LOL-Problem/m-p/1657354#M23277</link>
      <description>&lt;P&gt;Hi NXP,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; We found S32K312 will reset while&amp;nbsp; doing&lt;SPAN&gt;&amp;nbsp;(&lt;/SPAN&gt;&lt;EM&gt;ESD&lt;/EM&gt;&lt;SPAN&gt;)&lt;/SPAN&gt;&lt;EM&gt;Air discharge&lt;/EM&gt;&lt;SPAN&gt;&amp;nbsp;±15kV test. And we found reset reason is PLL_LOL. Then we use NXP S32K312EVB-Q172 to do the same test, it will reset too.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp;We try to change GM_SET register to improve&amp;nbsp;crystal diver strength,but it has no&amp;nbsp;improvement. And we try to set&amp;nbsp;DCMRWP3[9] to 1, S32K will not reset when PLL_LOL,but mcu will stop, only reset can recover it.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp;We need S32K3&amp;nbsp;keep running while the ESD test. Can cpu clock switch to FIRC while PLL_LOL? Could you give me some suggestions,Thanks!&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 25 May 2023 06:39:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-PLL-LOL-Problem/m-p/1657354#M23277</guid>
      <dc:creator>zhengjianfei1</dc:creator>
      <dc:date>2023-05-25T06:39:43Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 PLL_LOL Problem</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-PLL-LOL-Problem/m-p/1658413#M23333</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/172584"&gt;@zhengjianfei1&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Are you sure the FXOSC is that cause of the PLL Loss of Lock? Do you have the FXOSC clock monitor enabled?&lt;/P&gt;
&lt;P&gt;It could be just the PLL. Is the lastmile regulator enabled?&lt;/P&gt;
&lt;P&gt;You could try to change the system clock back to FIRC within the interrupt.&lt;/P&gt;
&lt;P&gt;MUX_0_CSC[SAFE_SW] = 1&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 26 May 2023 12:43:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-PLL-LOL-Problem/m-p/1658413#M23333</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2023-05-26T12:43:51Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 PLL_LOL Problem</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-PLL-LOL-Problem/m-p/1659424#M23382</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160001"&gt;@danielmartynek&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp; Thanks for your reply. CMU is disable and I am sure the reset reason is&amp;nbsp;&lt;SPAN&gt;PLL Loss of Lock. When PLL LOL,MCU will reset. When&amp;nbsp;set&amp;nbsp;DCMRWP3[9] to 1, mcu will not reset while PLL LOL but mcu will stop running. Thus we cannot&amp;nbsp;change the system clock back to FIRC when PLL LOL. We try to replace the&amp;nbsp;Crystal Oscillator with a higher-power one, it seems better.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 30 May 2023 03:08:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-PLL-LOL-Problem/m-p/1659424#M23382</guid>
      <dc:creator>zhengjianfei1</dc:creator>
      <dc:date>2023-05-30T03:08:29Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 PLL_LOL Problem</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-PLL-LOL-Problem/m-p/1660573#M23426</link>
      <description>&lt;P&gt;What do you mean by higher-power oscillator?&lt;/P&gt;
&lt;P&gt;Did you disable the automatic level controller (FXOSC_CTRL[ALC_D] = 1)?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;</description>
      <pubDate>Tue, 16 Sep 2025 07:24:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-PLL-LOL-Problem/m-p/1660573#M23426</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2025-09-16T07:24:31Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 PLL_LOL Problem</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-PLL-LOL-Problem/m-p/1665120#M23711</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;Daniel，&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; Thanks，disable&amp;nbsp;automatic level controller can slove this problem.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 07 Jun 2023 10:58:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-PLL-LOL-Problem/m-p/1665120#M23711</guid>
      <dc:creator>zhengjianfei1</dc:creator>
      <dc:date>2023-06-07T10:58:09Z</dc:date>
    </item>
  </channel>
</rss>