<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックLunching partition command on S32K</title>
    <link>https://community.nxp.com/t5/S32K/Lunching-partition-command-on-S32K/m-p/770652#M2325</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;STRONG&gt;Hi,&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I need to switch from HI_SPEED_RUN mode to Just RUN mode to lunch &lt;STRONG&gt;flash partition command&lt;/STRONG&gt; and back to hi speed run mode once done.&lt;/P&gt;&lt;P&gt;This is not working for me. use PE code to do this as fallows:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;POWER_SYS_Init(&amp;amp;powerConfigsArr, POWER_MANAGER_CONFIG_CNT, &amp;amp;powerStaticCallbacksConfigsArr, POWER_MANAGER_CALLBACK_CNT);&lt;/P&gt;&lt;P&gt;Where &lt;STRONG&gt;powerConfigsArr&lt;/STRONG&gt; is pointer to arrays of 2 configs (HI SPEED RUN, RUN)&amp;nbsp;and the CNT is 2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then to switch I do:&lt;/P&gt;&lt;P&gt;POWER_SYS_SetMode( 1, 0);&lt;/P&gt;&lt;P&gt;which is supposed to switch to RUN and then lunch the partition&amp;nbsp; command which generates a reset.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is wrong with this?&lt;/P&gt;&lt;P&gt;Please help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 13 Nov 2017 23:58:04 GMT</pubDate>
    <dc:creator>hajianik</dc:creator>
    <dc:date>2017-11-13T23:58:04Z</dc:date>
    <item>
      <title>Lunching partition command on S32K</title>
      <link>https://community.nxp.com/t5/S32K/Lunching-partition-command-on-S32K/m-p/770652#M2325</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;STRONG&gt;Hi,&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I need to switch from HI_SPEED_RUN mode to Just RUN mode to lunch &lt;STRONG&gt;flash partition command&lt;/STRONG&gt; and back to hi speed run mode once done.&lt;/P&gt;&lt;P&gt;This is not working for me. use PE code to do this as fallows:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;POWER_SYS_Init(&amp;amp;powerConfigsArr, POWER_MANAGER_CONFIG_CNT, &amp;amp;powerStaticCallbacksConfigsArr, POWER_MANAGER_CALLBACK_CNT);&lt;/P&gt;&lt;P&gt;Where &lt;STRONG&gt;powerConfigsArr&lt;/STRONG&gt; is pointer to arrays of 2 configs (HI SPEED RUN, RUN)&amp;nbsp;and the CNT is 2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then to switch I do:&lt;/P&gt;&lt;P&gt;POWER_SYS_SetMode( 1, 0);&lt;/P&gt;&lt;P&gt;which is supposed to switch to RUN and then lunch the partition&amp;nbsp; command which generates a reset.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is wrong with this?&lt;/P&gt;&lt;P&gt;Please help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Nov 2017 23:58:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Lunching-partition-command-on-S32K/m-p/770652#M2325</guid>
      <dc:creator>hajianik</dc:creator>
      <dc:date>2017-11-13T23:58:04Z</dc:date>
    </item>
  </channel>
</rss>