<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic reading signals from LIN bus in S32K</title>
    <link>https://community.nxp.com/t5/S32K/reading-signals-from-LIN-bus/m-p/1655908#M23211</link>
    <description>&lt;P&gt;Using an oscilloscope, I'm scoping the LIN pins to check that there is an rx and tx signal. I have an s32K344 board and I've connected the board to pins 2 and 8 of the LIN connector. I am currently running the Lin_Ip_FrameTransfer example project and I have not modified anything. When I run it, I get a flat line waveform but there are no changes to the waveform when I run it. What could be the issue/what modifications do I need to make?&lt;/P&gt;</description>
    <pubDate>Tue, 23 May 2023 16:40:36 GMT</pubDate>
    <dc:creator>cw20</dc:creator>
    <dc:date>2023-05-23T16:40:36Z</dc:date>
    <item>
      <title>reading signals from LIN bus</title>
      <link>https://community.nxp.com/t5/S32K/reading-signals-from-LIN-bus/m-p/1655908#M23211</link>
      <description>&lt;P&gt;Using an oscilloscope, I'm scoping the LIN pins to check that there is an rx and tx signal. I have an s32K344 board and I've connected the board to pins 2 and 8 of the LIN connector. I am currently running the Lin_Ip_FrameTransfer example project and I have not modified anything. When I run it, I get a flat line waveform but there are no changes to the waveform when I run it. What could be the issue/what modifications do I need to make?&lt;/P&gt;</description>
      <pubDate>Tue, 23 May 2023 16:40:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/reading-signals-from-LIN-bus/m-p/1655908#M23211</guid>
      <dc:creator>cw20</dc:creator>
      <dc:date>2023-05-23T16:40:36Z</dc:date>
    </item>
    <item>
      <title>Re: reading signals from LIN bus</title>
      <link>https://community.nxp.com/t5/S32K/reading-signals-from-LIN-bus/m-p/1656561#M23249</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;as example does communication between LIN Master/Slave on the board&amp;nbsp;connect J23.7 to J23.8 and place either J20 or J24 jumper. Then 2 LIN frames should be visible on LIN bus connection after example running.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="PetrS_0-1684923134330.png" style="width: 753px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/224693iA2ED9CDF9F703C01/image-dimensions/753x64?v=v2" width="753" height="64" role="button" title="PetrS_0-1684923134330.png" alt="PetrS_0-1684923134330.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Wed, 24 May 2023 10:14:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/reading-signals-from-LIN-bus/m-p/1656561#M23249</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2023-05-24T10:14:34Z</dc:date>
    </item>
    <item>
      <title>Re: reading signals from LIN bus</title>
      <link>https://community.nxp.com/t5/S32K/reading-signals-from-LIN-bus/m-p/1656769#M23256</link>
      <description>&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="cw20_0-1684941677200.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/224723i4AFD91C4110AC5FB/image-size/medium?v=v2&amp;amp;px=400" role="button" title="cw20_0-1684941677200.png" alt="cw20_0-1684941677200.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="cw20_1-1684941696549.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/224724i260B033D0EA0BA8B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="cw20_1-1684941696549.png" alt="cw20_1-1684941696549.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/52961"&gt;@PetrS&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;I have done what you said and when I run the example, I get a brief square wave and then it disappears. While debugging, I found that it stops at this point in the program: when waiting for transmission to be done on the slave (which I guess never happens). What could be the issue? Also, I am using the Lin_Ip_FrameTransfer example, should I be using Lin_MasterFrameTransfer instead?&lt;/P&gt;</description>
      <pubDate>Wed, 24 May 2023 16:22:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/reading-signals-from-LIN-bus/m-p/1656769#M23256</guid>
      <dc:creator>cw20</dc:creator>
      <dc:date>2023-05-24T16:22:38Z</dc:date>
    </item>
    <item>
      <title>Re: reading signals from LIN bus</title>
      <link>https://community.nxp.com/t5/S32K/reading-signals-from-LIN-bus/m-p/1657504#M23291</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;did you set master jumper as well on LIN transceiver. If you have LINs connected then you can place either J20 or J24, if not LIN2 is master in this example, I think and if J24 will be placed you should see LIN frame on J23.7.For latter case program stops at waiting for slave receive as slave is not connected.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Thu, 25 May 2023 08:55:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/reading-signals-from-LIN-bus/m-p/1657504#M23291</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2023-05-25T08:55:48Z</dc:date>
    </item>
  </channel>
</rss>