<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic USB-ML-UNIVERSAL-FX burn S32K314 error in S32K</title>
    <link>https://community.nxp.com/t5/S32K/USB-ML-UNIVERSAL-FX-burn-S32K314-error/m-p/1655204#M23162</link>
    <description>&lt;PRE&gt;Dear all,&lt;BR /&gt;&lt;BR /&gt;USB-ML-UNIVERSAL-FX burn S32K314 error, regardless of whether the target board &lt;BR /&gt;is connected or not, displays the attachment same error. already tried to set &lt;BR /&gt;it according to the "S32K3xx Secure Debug Support" ,but still displays the same &lt;BR /&gt;error. and the reset pin of the USB-ML-UNIVERSAL-FX always at low level. &lt;BR /&gt;The same target board can be burned successfully by replacing it with another &lt;BR /&gt;USB-ML-UNIVERSAL-FX. Could you help to advise what should we can set it? thank &lt;BR /&gt;you.&lt;BR /&gt;&lt;BR /&gt;Operating System: Windows 10 Enterprise Edition&lt;BR /&gt;software:S32 Design Studio for S32 Platform 3.4&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="error.png" style="width: 750px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/224321iA0518BAE9799E632/image-size/large?v=v2&amp;amp;px=999" role="button" title="error.png" alt="error.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;error.png&lt;/span&gt;&lt;/span&gt;&lt;/PRE&gt;</description>
    <pubDate>Tue, 23 May 2023 04:08:14 GMT</pubDate>
    <dc:creator>sunflower11</dc:creator>
    <dc:date>2023-05-23T04:08:14Z</dc:date>
    <item>
      <title>USB-ML-UNIVERSAL-FX burn S32K314 error</title>
      <link>https://community.nxp.com/t5/S32K/USB-ML-UNIVERSAL-FX-burn-S32K314-error/m-p/1655204#M23162</link>
      <description>&lt;PRE&gt;Dear all,&lt;BR /&gt;&lt;BR /&gt;USB-ML-UNIVERSAL-FX burn S32K314 error, regardless of whether the target board &lt;BR /&gt;is connected or not, displays the attachment same error. already tried to set &lt;BR /&gt;it according to the "S32K3xx Secure Debug Support" ,but still displays the same &lt;BR /&gt;error. and the reset pin of the USB-ML-UNIVERSAL-FX always at low level. &lt;BR /&gt;The same target board can be burned successfully by replacing it with another &lt;BR /&gt;USB-ML-UNIVERSAL-FX. Could you help to advise what should we can set it? thank &lt;BR /&gt;you.&lt;BR /&gt;&lt;BR /&gt;Operating System: Windows 10 Enterprise Edition&lt;BR /&gt;software:S32 Design Studio for S32 Platform 3.4&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="error.png" style="width: 750px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/224321iA0518BAE9799E632/image-size/large?v=v2&amp;amp;px=999" role="button" title="error.png" alt="error.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;error.png&lt;/span&gt;&lt;/span&gt;&lt;/PRE&gt;</description>
      <pubDate>Tue, 23 May 2023 04:08:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/USB-ML-UNIVERSAL-FX-burn-S32K314-error/m-p/1655204#M23162</guid>
      <dc:creator>sunflower11</dc:creator>
      <dc:date>2023-05-23T04:08:14Z</dc:date>
    </item>
    <item>
      <title>Re: USB-ML-UNIVERSAL-FX burn S32K314 error</title>
      <link>https://community.nxp.com/t5/S32K/USB-ML-UNIVERSAL-FX-burn-S32K314-error/m-p/1655646#M23194</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;it looks as the issue with the Multilink itself, especially if you tried different one and it works properly.&lt;BR /&gt;Check if the ribbon cable is placed properly within Multilink. Also consider driver/firmware version and if needed ask PEmicro support directly.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Tue, 23 May 2023 10:41:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/USB-ML-UNIVERSAL-FX-burn-S32K314-error/m-p/1655646#M23194</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2023-05-23T10:41:29Z</dc:date>
    </item>
    <item>
      <title>Re: USB-ML-UNIVERSAL-FX burn S32K314 error</title>
      <link>https://community.nxp.com/t5/S32K/USB-ML-UNIVERSAL-FX-burn-S32K314-error/m-p/1656131#M23224</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi, Petr,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;thanks for your advice and will try to check&amp;nbsp;&lt;SPAN&gt;driver/firmware.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Tina&lt;/P&gt;</description>
      <pubDate>Wed, 24 May 2023 02:07:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/USB-ML-UNIVERSAL-FX-burn-S32K314-error/m-p/1656131#M23224</guid>
      <dc:creator>sunflower11</dc:creator>
      <dc:date>2023-05-24T02:07:59Z</dc:date>
    </item>
  </channel>
</rss>