<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: What's different between “Can_MainFunction_Write” and &amp;quot;Can_Write&amp;quot; in s32k3? in S32K</title>
    <link>https://community.nxp.com/t5/S32K/What-s-different-between-Can-MainFunction-Write-and-quot-Can/m-p/1654804#M23149</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;yes, you are right.&lt;/P&gt;
&lt;P&gt;Can_Write checks TX MB if it is free to send data, if yes fills TX MB with data and transmit is initiated.&lt;/P&gt;
&lt;P&gt;Can_MainFunction_Write performs the polling of TX confirmation when CAN_TX_PROCESSING is set to POLLING. It checks MB flag if message was transmitted successfully or not, if yes updates driver variable and calls TXconfirmation.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
    <pubDate>Mon, 22 May 2023 11:59:42 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2023-05-22T11:59:42Z</dc:date>
    <item>
      <title>What's different between “Can_MainFunction_Write” and "Can_Write" in s32k3?</title>
      <link>https://community.nxp.com/t5/S32K/What-s-different-between-Can-MainFunction-Write-and-quot-Can/m-p/1654426#M23117</link>
      <description>&lt;P&gt;Can_Write see check hw state,but it has send message .&lt;/P&gt;&lt;P&gt;Can_MainFunction_Write see polling only, am I getting this right?&lt;/P&gt;</description>
      <pubDate>Mon, 22 May 2023 06:29:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/What-s-different-between-Can-MainFunction-Write-and-quot-Can/m-p/1654426#M23117</guid>
      <dc:creator>jingfang</dc:creator>
      <dc:date>2023-05-22T06:29:16Z</dc:date>
    </item>
    <item>
      <title>Re: What's different between “Can_MainFunction_Write” and "Can_Write" in s32k3?</title>
      <link>https://community.nxp.com/t5/S32K/What-s-different-between-Can-MainFunction-Write-and-quot-Can/m-p/1654804#M23149</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;yes, you are right.&lt;/P&gt;
&lt;P&gt;Can_Write checks TX MB if it is free to send data, if yes fills TX MB with data and transmit is initiated.&lt;/P&gt;
&lt;P&gt;Can_MainFunction_Write performs the polling of TX confirmation when CAN_TX_PROCESSING is set to POLLING. It checks MB flag if message was transmitted successfully or not, if yes updates driver variable and calls TXconfirmation.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Mon, 22 May 2023 11:59:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/What-s-different-between-Can-MainFunction-Write-and-quot-Can/m-p/1654804#M23149</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2023-05-22T11:59:42Z</dc:date>
    </item>
  </channel>
</rss>