<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックConflicting SDK driver files.</title>
    <link>https://community.nxp.com/t5/S32K/Conflicting-SDK-driver-files/m-p/1653552#M23068</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have S32DS project I am using S32K144.&lt;/P&gt;&lt;P&gt;I am&amp;nbsp;using S32 Design Studio for S32 Platform&lt;BR /&gt;Version: 3.5&lt;/P&gt;&lt;P&gt;When I am using config tools to generate peripheral, which gives the SDK that generate driver files but some driver files are already present in S32K144_SDK4.0.1 and that conflicting which gives multiple definition error.&amp;nbsp;&lt;/P&gt;&lt;P&gt;What will be the solution?&lt;/P&gt;</description>
    <pubDate>Fri, 19 May 2023 06:13:16 GMT</pubDate>
    <dc:creator>emb02</dc:creator>
    <dc:date>2023-05-19T06:13:16Z</dc:date>
    <item>
      <title>Conflicting SDK driver files.</title>
      <link>https://community.nxp.com/t5/S32K/Conflicting-SDK-driver-files/m-p/1653552#M23068</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have S32DS project I am using S32K144.&lt;/P&gt;&lt;P&gt;I am&amp;nbsp;using S32 Design Studio for S32 Platform&lt;BR /&gt;Version: 3.5&lt;/P&gt;&lt;P&gt;When I am using config tools to generate peripheral, which gives the SDK that generate driver files but some driver files are already present in S32K144_SDK4.0.1 and that conflicting which gives multiple definition error.&amp;nbsp;&lt;/P&gt;&lt;P&gt;What will be the solution?&lt;/P&gt;</description>
      <pubDate>Fri, 19 May 2023 06:13:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Conflicting-SDK-driver-files/m-p/1653552#M23068</guid>
      <dc:creator>emb02</dc:creator>
      <dc:date>2023-05-19T06:13:16Z</dc:date>
    </item>
    <item>
      <title>Re: Conflicting SDK driver files.</title>
      <link>https://community.nxp.com/t5/S32K/Conflicting-SDK-driver-files/m-p/1653633#M23073</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please use S32DS v3.4, it is mentioned in S32K1 SDK RTM 4.0.x release note.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 19 May 2023 08:01:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Conflicting-SDK-driver-files/m-p/1653633#M23073</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2023-05-19T08:01:28Z</dc:date>
    </item>
  </channel>
</rss>